This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO1540是否可以用来做CAN总线隔离?

Other Parts Discussed in Thread: ISO1540, ISO1050

ISO1540是如何判断数据流的方向,从而实现双向通信的?

是否也可以做CAN总线的隔离?如果可以需要注意哪些方面。

“通过将端 1 低电平输出电压偏移至一个大于端 1 高电平输入电压值,从而防止一个内部逻辑锁存(会出现在标准数字隔离器中)来在这些器件内实现隔离式双向通信。”

 如何理解?谢谢。