ISO1540是如何判断数据流的方向,从而实现双向通信的?
是否也可以做CAN总线的隔离?如果可以需要注意哪些方面。
“通过将端 1 低电平输出电压偏移至一个大于端 1 高电平输入电压值,从而防止一个内部逻辑锁存(会出现在标准数字隔离器中)来在这些器件内实现隔离式双向通信。”
如何理解?谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
首先双向注意只指的data线,clock只是单向的,关于数据的双向通信,可参考数据手册Page12 (Receive Direction和Transmitter Direction)的介绍。
不建议采用ISO1540做CAN总线的隔离,可选用ISO1050做CAN总线的隔离。http://www.ti.com/lit/ds/symlink/iso1050.pdf