This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB960-Q1: DS90UB960输入数据量和输出端怎么分享带宽

Part Number: DS90UB960-Q1

你好,960的输入端支持4路FPD_LINK最多共计 4.16Gbps 数据量输入,每一路FPDlink有最大数据量限制么?比如只采用2路输入,一路数据量1920*1080*60*16*1.2=2.38Gbps, 另外一路大概1.4Gbps,只有可以么?  另外,输出端的两路CSI2都使用,采用分享带宽(不是复制,两路输出数据不一样),这个是怎么设置的,手册哪里有讲到么?

  • 960的输入端支持4路FPD_LINK最多共计 4.16Gbps 数据量输入,每一路FPDlink有最大数据量限制么?比如只采用2路输入,一路数据量1920*1080*60*16*1.2=2.38Gbps, 另外一路大概1.4Gbps,只有可以么?

    您好,每路FPD link的最大数据吞吐量的限制是和您搭配使用serializer有关,只要serializer支持,对于960来说只要不超过4.16Gbps就没问题.

    输出端的两路CSI2都使用,采用分享带宽(不是复制,两路输出数据不一样),这个是怎么设置的,手册哪里有讲到么?

    这个应该是不需要设置的,960输出每路CSI-2的最大带宽为1.664*4=6.656Gbps,960是四路独立的通道输入,然后通过分配虚拟通道然后整合到CSI-2输出,只要960的输出能力满足需求即可。这里有一篇关于深入理解FPD link速率的应用手册,讲的很详细 ,您参考下:

    https://www.ti.com.cn/cn/lit/an/zhcaa76/zhcaa76.pdf

  • 960四路FPDLINKIII输入,每一路只要不超过4.16Gbps就没问题么?而不是四路加起来合计不能超过4.16Gbps吧?   另外,如果两路FPDlinkIII a,b输入,两路CSI2接口(A和B)都输出,如何配置为让a对应A,  b对应B?

  • 是的,4.16Gbps指的是每路RX 的line rate能达到4.16Gbps,不是总的。

    如果两路FPDlinkIII a,b输入,两路CSI2接口(A和B)都输出,如何配置为让a对应A,  b对应B?

    这个可以参考7.4.18.1 Example 1。 它是采用了4路,如果采用两路的话,每一路使用虚拟ID VC-ID 0 发送,配置960映射输入进来的VC-ID保证每一路都有一个唯一的ID。RXport0 对应VC-ID0,RXport1对应VC-ID1. 另外,RX port0 被分配到CSI TX0,RX port1 被分配到CSI TX1. 

    具体您可以参考下数据手册P41的示例:https://www.ti.com.cn/lit/ds/symlink/ds90ub960-q1.pdf