This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB947-Q1: 941,941透传PWM控制

Part Number: DS90UB947-Q1

Hi ,

       你好!

      外部的MCU有个PWM(频率6k)需要通过941,传输到948输出。用的是GPIO1。

941参数如下:

{0x0E,0x33},

948参数如下:

{0x1E,0x55},

948输出一直为高,不能随941的输入而变化。请问还需要怎么设置?

谢谢!

  • 941参数如下:

    {0x0E,0x33},

    941的GPIO作为输入,应该使用back channel 因此0x0E[3:0] = 0x5,bit[7:4]是配置GPIO2的,您使用的GPIO1,所以bit[7:4] 我们可以使用默认值为0

    即0x0E=0X05

    948参数如下:

    {0x1E,0x55},

    948的GPIO作为输出,所以使用的是forward channel。所以0x1E[3:0] = 0x5。 同样,您使用的GPIO1,所以bit[7:4] 我们可以使用默认值为0

    即0x1E=0x05.

    您试试,看是否能透传?