Hi Kailyn Chen ,
你好!
外部的MCU有个PWM(频率6k)需要通过941,传输到948输出。用的是GPIO1。
941参数如下:
{0x0E,0x33},
948参数如下:
{0x1E,0x55},
948输出一直为高,不能随941的输入而变化。请问还需要怎么设置?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Kailyn Chen ,
你好!
外部的MCU有个PWM(频率6k)需要通过941,传输到948输出。用的是GPIO1。
941参数如下:
{0x0E,0x33},
948参数如下:
{0x1E,0x55},
948输出一直为高,不能随941的输入而变化。请问还需要怎么设置?
谢谢!
941参数如下:
{0x0E,0x33},
941的GPIO作为输入,应该使用back channel 因此0x0E[3:0] = 0x5,bit[7:4]是配置GPIO2的,您使用的GPIO1,所以bit[7:4] 我们可以使用默认值为0
即0x0E=0X05
948参数如下:
{0x1E,0x55},
948的GPIO作为输出,所以使用的是forward channel。所以0x1E[3:0] = 0x5。 同样,您使用的GPIO1,所以bit[7:4] 我们可以使用默认值为0
即0x1E=0x05.

您试试,看是否能透传?