Part Number: SN65LVDS348
sn65lvds348的供电电压只有3.3v,为什么它的输出电压可以达到6v,在实际应用中怎么固定输出电压的大小呀?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65LVDS348
sn65lvds348的供电电压只有3.3v,为什么它的输出电压可以达到6v,在实际应用中怎么固定输出电压的大小呀?
您的意思是您需要使用SN65LVDS348的3个输出分别去驱动3个输入?
1、这个开关的控制电压是上面表格中的control voltage low 范围 0~0.5V 和 control voltage high 范围是2.7V ~VDD 吗?您使用的VDD是3.3V 是吗?
如果是这样的话,这是没问题的,因为SN65LVDS348在供电电压3.3V时,在输出高电平输出5uA时,根据Figure 9,其输出电压约为3.3V,也就是说电压降很小;即使输出电流5mA时,输出电压是3V,也大于开关 Mini circuit ZFSWA2-63DR+要求的最小电压2.7V,且输出电流远高于需要的5uA;

2、
2、当我接3路输出,那么是唯一的一个电压源驱动这三个,还是有3电压源分别驱动?
这里是什么意思?电压源指哪里的电压源?
3、SN65LVDS348不可以5V供电,其供电范围是3V ~3.6V