This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65LVDS348: 输出电压最大可以是多少,怎么设置输出电压大小

Part Number: SN65LVDS348


sn65lvds348的供电电压只有3.3v,为什么它的输出电压可以达到6v,在实际应用中怎么固定输出电压的大小呀?

  • 您好,

    它不能输出6V电压,这是ABSOLUTE MAXIMUM RATINGS(绝对最大额定值)表格中的参数,这里的意思是这些管脚可以承受最大6V的过应力而不损坏,输出电压高低电平如下截图所示,最低高电压是2.5V;最大低电平电压是0.4V,具体输出电压与输出电流有关,如下截图关系曲线:

  • 您好,那我如何确定输出电压大小呀?如果我想固定输出高电平3.3v,低电平0v,那我的外围电路需要单独设置么?

  • SN65LVDS348没办法固定输出电压,它受输出电流的影响,若供电3.3V,欲输出高电平3.3v,低电平0v,那么输出电流就需要是0,也就是后端没有负载;

    如果您需要输出完全达到电源轨,那么需要外加电路进行调节了;您需要的驱动电流是多少?您可以容忍的对电源轨的电压最大是多少?

  • Hi Amy,我这边需要接三个输出,但是我只找到其中一个的参数表Mini circuit ZFSWA2-63DR+,我还有以下几个问题:

    1、表中显示这个开关需要5uA的驱动电流,那么我实际输出的是多大电压呀?

    2、当我接3路输出,那么是唯一的一个电压源驱动这三个,还是有3电压源分别驱动?

    3、我的供电电压可以不是3,3v,换成5v可以么?

  • 您的意思是您需要使用SN65LVDS348的3个输出分别去驱动3个输入?

    1、这个开关的控制电压是上面表格中的control voltage low  范围 0~0.5V 和 control voltage high  范围是2.7V ~VDD 吗?您使用的VDD是3.3V 是吗?

    如果是这样的话,这是没问题的,因为SN65LVDS348在供电电压3.3V时,在输出高电平输出5uA时,根据Figure 9,其输出电压约为3.3V,也就是说电压降很小;即使输出电流5mA时,输出电压是3V,也大于开关 Mini circuit ZFSWA2-63DR+要求的最小电压2.7V,且输出电流远高于需要的5uA;

    2、

    2、当我接3路输出,那么是唯一的一个电压源驱动这三个,还是有3电压源分别驱动?

    这里是什么意思?电压源指哪里的电压源?

    3、SN65LVDS348不可以5V供电,其供电范围是3V ~3.6V