Other Parts Discussed in Thread: DP83620
请问DP83620 用光口 需要怎么配置? 我有DP83848程序 测试好用。 直接用在DP83620光口 好用吗? 不行的话需要改些什么? 谢谢了 MAC层的接口是RMII。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: DP83620
请问DP83620 用光口 需要怎么配置? 我有DP83848程序 测试好用。 直接用在DP83620光口 好用吗? 不行的话需要改些什么? 谢谢了 MAC层的接口是RMII。
如果需要用光口的话,有两种配置模式:power-up/reset时讲RX_ER pin下拉;或者通过寄存器配置。、
具体的寄存器你需要和DP83848对比下,它们是不是一致的。
The DP83620 supports both Twister Pair (100BASE-TX and 10BASE-T) and Fiber (100BASE-FX) media.
The port may be configured for Twisted Pair (TP) or Fiber (FX) operation by strap option or by register
access.
At power-up/reset, the state of the RX_ER pin will select the media for the port. The default selection is
twisted pair mode, while an external pull-down will select FX mode of operation. Strapping the port into FX
mode also automatically sets the Far-End Fault Enable, bit 3 of PCSR (16h), the Scramble Bypass, bit 1
of PCSR (16h) and the Descrambler Bypass, bit 0 of PCSR (16h). In addition, the media selection may be
controlled by writing to bit 6, FX_EN, of PCSR (16h).
DP83620 光口的 例程 给我发一下 859950606@qq.com 十分谢谢 !
不好意思,我手上没有相关的例程,因为这是和MCU相关的。
不需要具体的例程 就是都需要配置哪些寄存器就行, 我自己配置了一些 没好用。