This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

急!!!请问DP83620 用光口 需要怎么配置?帮帮忙 十分感谢

Other Parts Discussed in Thread: DP83620

请问DP83620 用光口  需要怎么配置?  我有DP83848程序  测试好用。 直接用在DP83620光口  好用吗? 不行的话需要改些什么?  谢谢了    MAC层的接口是RMII。

  • 如果需要用光口的话,有两种配置模式:power-up/reset时讲RX_ER pin下拉;或者通过寄存器配置。、

    具体的寄存器你需要和DP83848对比下,它们是不是一致的。

    The DP83620 supports both Twister Pair (100BASE-TX and 10BASE-T) and Fiber (100BASE-FX) media.
    The port may be configured for Twisted Pair (TP) or Fiber (FX) operation by strap option or by register
    access.
    At power-up/reset, the state of the RX_ER pin will select the media for the port. The default selection is
    twisted pair mode, while an external pull-down will select FX mode of operation. Strapping the port into FX
    mode also automatically sets the Far-End Fault Enable, bit 3 of PCSR (16h), the Scramble Bypass, bit 1
    of PCSR (16h) and the Descrambler Bypass, bit 0 of PCSR (16h). In addition, the media selection may be
    controlled by writing to bit 6, FX_EN, of PCSR (16h).

  • DP83620 光口的 例程    给我发一下    859950606@qq.com   十分谢谢 !

  • 不好意思,我手上没有相关的例程,因为这是和MCU相关的。

  • 不需要具体的例程    就是都需要配置哪些寄存器就行,  我自己配置了一些   没好用。

  • 同求啊,,我也用的83620这个片子,也是想用光口功能,都是用的管脚STRAP  PIN的,不知道可不可以啊,我的光口也不通啊。。。

    需要配什么寄存器呢。。