Other Parts Discussed in Thread: DS90UB947-Q1,
DS90UB947-Q1与DS90UB948-Q1使用,进行pattern test,屏幕无显示。
根据snla132g文档中4.4案例进行配置 使用without FPD-Link III方案,配置948进入pattern test直接输出屏幕无显示,屏幕有背光。
我该如何进行判断是哪里出现的问题,请给予回复,十分感谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,屏幕无显示,那948输出是否有波形?用示波器测量下输出是否有信号或者波形?
另外,注意4.4案例中的配置只能是配置在dual link模式下的示例。
0x28 bit4 =1 enable dual link mode

另外,读取下寄存器0x69 bit7,看是否有Pattern BIST error。
还需要注意的是,0x63必须配置为0x01,在pattern test时bit0=1 power down CML TX。
我看应用手册的4.4示例没有列举出来。