Part Number: DS90UB921-Q1
主机端已经可以获取到触摸屏数据,触摸屏的中断信号接在了948的BISTC / INTB_IN,通过lvds传输给921, 921通过INTB引脚接到到主机。
如何将948的BISTC / INTB_IN信号透传给921(948的信号发生变化,921也会发生信号变化)?

948的硬件连接:


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB921-Q1
主机端已经可以获取到触摸屏数据,触摸屏的中断信号接在了948的BISTC / INTB_IN,通过lvds传输给921, 921通过INTB引脚接到到主机。
如何将948的BISTC / INTB_IN信号透传给921(948的信号发生变化,921也会发生信号变化)?

948的硬件连接:


您好,是不是使用的GPIO进行透传?也即是将948的GPIO配置为输入,921的GPIO配置为输出?
触摸屏的中断信号已经接在了948的BISTC / INTB_IN上了,921需要怎么配置才可以获取948这个信号的透传
抱歉,这个问题不知什么原因没有看到需要跟进。 非常抱歉。
我马上看下您的问题,稍后给您回复。
您好,参考921的数据手册7.3.13部分关于interrupt的介绍,REM_INTB可以镜像remote deserializer端的INTB_IN信号。任何remote Des端的INTB_IN的变化都会反映到REM_INTB端。或者也可以通过下面的配置步骤使用921的INTB设置为在远程上的触发。但我理解的是这个和透传是不一样的,如果需要透传,就像您提到的,触摸屏的中断信号的变化,921这边也会发生相应的变化,这个需要GPIO引脚来实现。