This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问DS90UB948 的LVDS输出有没有展频功能,如果有,怎么打开或设置?
备注:现在做EMC RE测试,确认是LVDS时钟超了很多,
串行器用的是DS90UB941
您好,是这样的。 我们的这些FPD link器件内部是没有SSC clock Gen的,所以只有当输入源提供了展频的时钟信号给serializer,并且Ser端是支持展频的,那么Deserializer端也是展频输出。DS90UB941AS的数据手册里有介绍SSC,最大展频为0.5%。所以我们通常在应用的时候,如果不使用展频或者最小的展频是否符合您的EMI要求? 不知您需要搭配使用的serializer型号是什么,如果是941的话,941AS/948具有强大的系统设计和物理屏蔽功能,无需使用任何 SSC 即可满足大多数 EMC 要求。
您好
.serializer型号是DS90UB941,941的输入是MIPI信号,MIPI的信号开不了展频吧?
是的,941自己本身无法打开展频,需要视频源提供给941已经开展频的clock。
RE测试不通过,想和您确认下PCLK是如何提供给948的? 是否已经关掉背光测试?
因为我们对948的EMC测试是没问题的。