Dear TI:
1:有两颗2M@60fps的摄像头Sensor,需要传输RAW格式的数据给SOC,传输距离5m,请帮忙评估使用DS90UB935/936是否可以(理论计算RAW模式带宽是够的)?POC的传输速率大约为多少?需要注意什么?
2:使用POC传输电源,对电流是否有限制?远端摄像头模组耗流约12V@200mA
3: 如果使用四颗摄像头,并且要做帧同步功能,是否可以用两颗936解串?
谢谢~~~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear TI:
1:有两颗2M@60fps的摄像头Sensor,需要传输RAW格式的数据给SOC,传输距离5m,请帮忙评估使用DS90UB935/936是否可以(理论计算RAW模式带宽是够的)?POC的传输速率大约为多少?需要注意什么?
2:使用POC传输电源,对电流是否有限制?远端摄像头模组耗流约12V@200mA
3: 如果使用四颗摄像头,并且要做帧同步功能,是否可以用两颗936解串?
谢谢~~~
1. FPD link传输具体的上限大概在15~20m。 请参考e2e.ti.com/.../ds90ub941as-q1-what-is-the-upper-limit-of-the-fpd-link-cable-s-transmisson-distance。
所以要计算下带宽是否够,如果带宽没问题,则可以考虑935和936.
使用POC传输电源,对电流是否有限制?远端摄像头模组耗流约12V@200mA
datasheet推荐低于150mA。

3. 935和936都是一路的,如果您需要接四颗摄像头,可以直接考虑使用4路DS90UB960这款解串器。

Dear TI:
感谢回复,935的规格描述支持到1M@60fps,我们的应用为2M@60fps,所以不确认是否OK。
935 的 CSI-2 接口单 lane 最大也能够支持 832Gbps,但是 CSI-2 port 总带宽能支持到 2.528Gbps,不像953,CSI-2 最大 Bandwidth能支持到 3.328Gbps。
所以我们可以根据您的实际应用计算下需要的总带宽,是什么数据格式,RAW还是YUV422或其他格式?然后根据2M@60fps具体计算一下。
我们的需求为远端的摄像头传输2M@60fps的RAW12格式数据,CSI数据线为2lane,请帮忙评估935是否够用。
2M@60fps 是不是1600*1280的分辨率? 那我们可以计算下总的带宽:
1600*1280*60*12*(1+25%)=1.843Gbps,而935最大能支持的带宽是2.528-Gbps,1.843Gbps<2.528Gbps.
所以935是支持2M@60fps的RAW12的。