請問CAN BUS若持續有訊號輸出,nINT會持續一直送中斷訊號嗎?
目前測試CAN BUS一直送訊號,約8小時後,nINT腳位會由active 狀態變為low,
以示波器測量CAN BUS仍有訊號,但因為nINT腳位狀態為low就不再收資料,
nINT腳位可以設定一直active嗎?還是多久時間後TCAN4550需要RST?
如何測量得知目前TCAN4550是Normal mode or sleep mode?謝謝.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
請問CAN BUS若持續有訊號輸出,nINT會持續一直送中斷訊號嗎?
目前測試CAN BUS一直送訊號,約8小時後,nINT腳位會由active 狀態變為low,
以示波器測量CAN BUS仍有訊號,但因為nINT腳位狀態為low就不再收資料,
nINT腳位可以設定一直active嗎?還是多久時間後TCAN4550需要RST?
如何測量得知目前TCAN4550是Normal mode or sleep mode?謝謝.
1、看寄存器值,好像是SPI出现了error。这里建议您先着重检查SPI通信;
2、寄存器16'h0800 bit8您设置的是什么?这一位决定了nWKRQ pin 功能:

low power CAN RX应该是指的下面绿色框内部分,我用红色框框起来的那部分,可以检测RXD_INT。RXD_INT是内部信号路径,其行为方式类似于物理层收发器的RXD引脚。在正常操作期间,外部引脚无法接触到它们。TCAN4550提供了将这些信号映射到外部引脚的Test Mode,请参阅datasheet 8.4.4 Test Mode。


WD是watchdog function,下面文档中有看门狗功能描述和应用示例:
https://www.ti.com/lit/ug/sllu270/sllu270.pdf