按照芯片手册配置爆震芯片后,在不接入爆震信号的情况下,芯片out脚有持续信号输出。
图1为销售提供芯片手册,按示例配置。 图2 紫线为窗口信号,蓝线为爆震芯片out脚信号,绿线为模拟输入的爆震信号
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
为更加有效地解决您的问题,我已将您的问题发布在E2E英文技术论坛上,请更了解这款芯片的TI资深工程师为您解答,一旦得到回复后我会立即回复给您。帖子链接如下,您也可以关注帖子,以方便查看或追问后续疑问。
收到E2E英文论坛工程师如下回复:
A little more detail would help us understand the problem.
1. Is the customer using our EVM, or their own PCB?
- If it is their PCB, can they provide a schematic & layout?
2. Can they provide their device settings?
3. What does the customer expect to see with their waveforms?
1.您是使用的EVM还是自己设计的PCB?
如果是自己设计的PCB,可以提供您的原理图和PCB layout吗
2.可以提供设备设置吗?
3.您期望在波形中看到什么?
很抱歉,技术支持都是在论坛上进行的:
中文技术论坛:https://e2echina.ti.com/
英文技术论坛:https://e2e.ti.com/
为更加有效地解决您的问题,我已将您的问题发布在E2E英文技术论坛上(见上面第一个回复中的链接),请更了解这款芯片的TI资深工程师为您解答。
由于时差问题,美国的工程师一般都是北京时间的晚上进行回复,为提供沟通效率,您也可以关注帖子、在上述英文论坛链接上直接与美国的工程师回复沟通。
Hi, 首先对此延迟回复深表歉意!
如果您有EVM,您是否可以配置成与您的电路板一样,然后在相同条件下查看是否可以看到输出信号?
如果没有EVM,请您尝试做以下操作:
1、爆震传感器是否连接至TPIC8101 还是断开的?
2、如果是连接的,断开连接是否会更改输出?
3、检查断开的KNOCK_H 和KNOCK_L上的信号/噪声
4、检查VCC和VREF线路上是否有噪声
5、将KNOCK_H 和 KNOCK_L短接在一起,
-这是否会改变输出信号?