Other Parts Discussed in Thread: TUSB212,
TUSB211、TUSB212是否可以支持外部标准USB DM信号接到D1P,PCB直连到D2P后再接到外部DM信号? 外部USB DP网络----芯片D1M引脚----芯片D2M引脚---外部USB DP网络,这样接有没有问题?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,没问题,TUSB211的DP, DM的极性可以交换,即您的应用外部USB DP网络----芯片D1M引脚----芯片D2M引脚---外部USB DP网络
或者DP(Host)-------D1M---D2M--------DP (Device)。只要host和device之间,或者两端外部USB网络的极性一致就好。
是否TUSB211和TUSB212都可以交换极性来用?另外,TUSB212是不是可以完全取代TUSB211?
是否TUSB211和TUSB212都可以交换极性来用
是的可以,都可以交换DP和DM的极性。
TUSB212是不是可以完全取代TUSB211?
您好,TUSB212和211相比,212由于增加了eDC_BOOST,所以相比211有着更好的redriver性能,
另外,二者的引脚对应差异如下:

可参考这篇211和212电气参数对比的应用手册:
https://www.ti.com/lit/an/slla376/slla376.pdf