This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB948-Q1: LOCK初期上电抖动

Part Number: DS90UB948-Q1


您好,TI

现在上电过程中出现LOCK抖动现象,请见测试波形

测试波形:/resized-image/__size/320x192/__key/communityserver-discussions-components-files/59/tek00012.png

1. LOCK信号在初期上电时,会出现抖动,后期持续为高,造成的原因是什么?

2. 初期上电LOCK抖动这是FPD-LINK的固有问题吗?TIEVM板的LOCK是否也有抖动情况?

3. 按照我们的架构,LOCK为低的时候,可以对948进行初始配置吗?可以对948slave设备进行I2C配置吗?

block:/resized-image/__size/320x240/__key/communityserver-discussions-components-files/59/block.PNG
4. 通常9480x02寄存器初期化应该配置成什么值?bit5是只有自检的时候需要用吗?

5. 看LOCK的状态表,948的0x02的bit4和bit7需要置H,需要在初始化时候配置吗?