This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1、应用场景如上图,941的输入为单路MIPI DSI0(1080p60Hz),和解串器948通过dual fpd-link传输。目前在941上面开启internal pattern后,LCD上能看到正确的color bar画面。——这能说明FPD链路、解串器配置、LCD驱动这些都是正常的。
2、关闭internal pattern后,LCD上无画面显示。问题应该出在SOC输入给941的MIPI DSI0上面。我们检查了SOC配置的MIPI DSI的timing,和internal pattern是一致的。
3、接下来应该如果排查问题呢?941上面是否有相关寄存器能指示出问题所在呢?
Thanks!
您好,可以读取下948的状态寄存器,我的电脑原因,数据手册暂时打不开,我记得是0x4D,您看下,先看下948这里是否能有效收到前端941输出的数据?是否符合pass标准?另外948输出lock引脚什么电平?
抱歉寄存器我记错了。
那从您读取的寄存器的值来看,问题并不出在SOC输入给941的MIPI DSI0上面。
948的寄存器0x02您是怎么配置的。参考Table7-1的配置。 确认下948的输出是否被disable/sleep.