This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI team,
这边想咨询一下有关DS125MB203的问题。目前我们使用该芯片应用与HDMI2.1输入的设计中,在两种HDMI2.1的线中存在不同的情况,一种为1m长的belkin HDMI2.1线(左图),另一种为右图所示的1.5米长的HDMI2.1线。现发现在常温下使用右图所示的线存在数据信号失锁不稳定的现象,而使用belkin HDMI2.1线则稳定;初次排查认为是EQ设置问题,根据芯片手册Table2对EQ值进行重新调配,发现EQ值确会对接受数据有影响,但没有合适的EQ值使该现象稳定正常,目前有如下几个问题想咨询:
谢谢!
您好,
很抱歉回复晚了!
您是使用的什么模式?Pin Control Mode 吗?那么应该根据Table3设置DEM、VOD,在Pin Control模式下,VOD是自动调节的。
1、ENSMB=1的话,EQ、DEM、VOD参数都由寄存器分别控制,EQ、DEM、VOD参数都是用来调节信号的,在对传输信号质量调节的时候都需要考虑;
2、每个CH线缆走线可能是一样的,但PCB走线可能不一样,因此每个ch都有对应的配置寄存器,那么不同的走线信号质量可能就不一样,需要补偿的参数也就可能不一样,因此寄存器配置可能就不一样;
3、在SMBUS模式下,EQ、DEM、VOD参数都由寄存器控制,其它外部控制引脚各自的寄存器如果是默认值的话,那么它们采用的是Pin Control Mode。
目前我们使用belkin的2m线低温存在闪屏现象,通过将EQ、VOD、DEM的值调为level1可使其在低温稳定,但使用belkin的1m线设置相同的值还存在闪屏现象,且尝试多个level的值并无改善现象,请问有什么调试建议吗?(目前调试时将所有CH的EQ值都设为同一level的值,VOD及DEM随EQ的level对应设置)
很抱歉回复晚了
在大多数应用中,我们一般建议从最低EQ,DEM=0dB,VOD=1000mV 设置开始,然后检测眼图以调整EQ和DEM设置来获得最佳眼图。
该芯片没有自动均衡的功能。