This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB3.0 controller (TUSB7320) 在Win2K8下加载驱动失败,USB3.0接口不能使用



1. 设计:

Romley-EP 2S平台,PCH(C602J) 的PCIE信号经PCIE 2.0 redriver拉到前面板的USB3.0.

2. 问题:

测试发现DOS下2个USB3.0 port可以正常使用。

进入OS后,先安装chipset driver,然后安装USB3.0 controller driver (Texas_Instruments_xHCI_Driver_v1.16.3_WHQL),但是驱动不能成功加载,有黄色感叹号出现。

卸载并重新安装驱动,在Device Manager下发现"Texas Instruments XHCI Controller”上依然有黄色感叹号出现(可参考附图),同时看不到"Texas Instruments USB Root Hub"项。

请帮忙判断分析可能是哪方面原因?多谢!

USB3.0 controller驱动加载失败截图-20131011A.doc