This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,DP83849IF的硬件复位时间在1ms以上即可正常复位了,因此肯定不是复位时间段的问题,你可以看一下MAX809的输出脉冲的幅度,看看是否属于TTL电平范围的高低
谢谢您的回复,我又检查了一下,发现DP83849IF不管是不是使用MDC/MDIO,好像是必须有MDC信号,之前因为FPGA还没有设计,才没有MDC信号,现在在FPGA写点逻辑,加一个5MHz的MDC信号,芯片就正常了,管理接口是必须要加么?
你好,是的,datasheet 上page47有:The DP83849IF requires a single initialization sequence of 32 bits of preamble following
hardware/software reset. This requirement is generally met by the mandatory pull-up resistor on MDIO in
conjunction with a continuous MDC, or the management access made to determine whether Preamble
Suppression is supported.