This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear TI:
下面是我的系统框图:
sensor A: 2 Lanes, 445.5Mbps/Lane, 1920 x 1080@30fps. VC-ID: 0
sensor B: 2 Lanes, 445.5Mbps/Lane, 1920 x 1080@30fps. VC-ID: 1
953: 4 Lanes, 800Mbps/Lane
954: 2 Lanes, 1.6Gbps/Lane
ISP: Qualcomm ISP.
当我先打开sensor A,正常出预览后,再打开sensor B,这时 ISP 会上报如下 mipi 错误。请问是不是954的CSI replicate Mode 改变了 sensor 数据?该如何 调试 CSI replicate Mode 的数据?
[ 216.708758] CAM_ERR: CAM-ISP: cam_ife_csid_irq: 5137 CSID:1 UNBOUNDED_FRAME: Frame started with EOF or No EOF
[ 216.708766] CAM_ERR: CAM-ISP: cam_vfe_bus_error_irq_top_half: 2651 Bus Err IRQ
[ 216.708778] CAM_ERR: CAM-ISP: cam_vfe_bus_error_irq_top_half: 2655 vfe:1: IRQ_Status0: 0x4000
[ 216.708783] CAM_INFO: CAM-ISP: cam_ife_csid_irq: 5145 CSID: 1 Error IRQ Count:1
[ 216.708790] CAM_ERR: CAM-ISP: cam_vfe_bus_error_irq_top_half: 2655 vfe:1: IRQ_Status1: 0x0
[ 216.708795] CAM_INFO: CAM-ISP: cam_ife_csid_irq: 5305 CSID:1 IPP_PATH_ERROR_CCIF_VIOLATION: Bad frame timings
[ 216.708802] CAM_ERR: CAM-ISP: cam_vfe_bus_error_irq_top_half: 2655 vfe:1: IRQ_Status2: 0x0
[ 216.708806] CAM_INFO: CAM-ISP: cam_ife_csid_irq: 5469 CSID:1 RDI :1 PATH_ERROR_CCIF_VIOLATION: Bad frame timings
[ 216.708865] CAM_ERR: CAM-ISP: cam_ife_csid_irq: 5137 CSID:2 UNBOUNDED_FRAME: Frame started with EOF or No EOF
[ 216.708872] CAM_INFO: CAM-ISP: cam_ife_csid_irq: 5145 CSID: 2 Error IRQ Count:7
[ 216.708877] CAM_ERR: CAM-ISP: cam_vfe_bus_err_bottom_half: 1460 Bus Violation: debug_status_0 = 0x2
[ 216.708890] CAM_INFO: CAM-ISP: cam_vfe_bus_err_bottom_half: 1466 RDI 1 violation
[ 216.708925] CAM_ERR: CAM-ISP: __cam_isp_ctx_handle_error: 2488 Error with no active/wait request
[ 216.709009] CAM_WARN: CAM-ISP: __cam_isp_ctx_handle_error: 2643 Notify CRM: req 0, frame 1 ctx 0, error 2
谢谢~
当我先打开sensor A,正常出预览后,再打开sensor B,这时 ISP 会上报如下 mipi 错误
您好,再打开sensorB 的时候,sensor A 也是enable状态,还是disable了?
954的replicated mode是针对要么一路sensor输入,输出两路CSI port,一路可以为replicated mode。
或者是两路sensor同时打开,将输入源整合到一起,然后输出两路,一路为replicated mode。
您好,再打开sensorB 的时候,sensor A 也是enable状态,还是disable了?
此时,sensor A 是 enable 状态的,所以目前怀疑是不是 这种操在replicated mode 时 会对 数据流有影响?
您好,我看您也同步了在E2E上的回复。 因为replicated mode是要么输入一路sensor(我看您E2E的反馈是,只enable 一路sensor 是可以正常工作的),要么同时输入两路sensor 整合两路视频再输出replicated mode。
您的这种应用,先enable一路,再enable一路,不同时打开的这种模式,需要和E2E确认一下。