This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

想请TI工程师评估下928的应用方案

我们的设想是通过 MCU-925-928的一个通道,MCU直接对928的GPIO口进行操作产生PWM信号,这样是可行的吗?

预想中:MCU对928的GPIO操作产生PWM时,其它操作是不可能进行的?因为通信通道被占用了,这样理解没错吧?

 我们的LVDS通道上的数据有:I2C控制信号,视频信号,触摸屏的中断及RESET信号

按你们经验,这样的方案是可行的吗?

方案构架:MCU+925+928+LCD+TP(触摸屏)

方案描述:1、视频信号同925和928的LVDS通道完成传输,输送到LCD

2、TP数据由I2C通道接到928,然后通过928的LVDS通道和MCU通信

3、TP RESET、背光的PWM信号、背光的电源开关控制信号连接到928的GPIO,由MCU对928 的GPIO操作,完成这些信号的控制

4、TP的中断信号通过928的中断PIN输入,925的中断PIN输出,传送到MCU,完成TP的中断响应

能不能帮忙评估下以上方案的可行性,或者有什么漏洞。

再次麻烦您了,谢谢!

祝工作愉快

  • 看来你对925/928比较了解。整个设想没有大的问题。

    唯一可能会有问题的是:MCU对928 GPIO操作输出PWM信号, 可以这么做,但是会占用很多系统资源。I2C的速率只能在 50K左右。

    如果只传18比特视频,就可以传PWM信号。