This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCE62005的AUX_IN接的晶振负载电容改选择多少pF的?

Other Parts Discussed in Thread: CDCE62005

专家,您们好!

CDCE62005的datasheet中说aux_in内部是10pF的谐振电容,见图

CDCE62005的EVM中没有给出他选择的晶振负载电容是多少,但是EVM在晶振的外部并联了一个5pF的电容,

TMDSEVM6678的开发板中用到了CDCE62005,他选择的晶振负载电容是20pF的,外部没有并联电容,所以想请教下,CDCE62005的AUX_in到底应该接多大负载电容的晶振?

谢谢!

  •  是的,CDCE62005的aux_in内部是10pF的谐振电容,晶振连接时,正确的做法是一个脚连在AUX_IN端,另一个脚接地,并联电容的大小为(CL-10)pF,,CL为晶振的负载电容大小,可通过晶振的datasheet中查到。

  • 首先谢谢Karlyn chen,

          如您的回答: 正确的做法是一个脚连在AUX_IN端,另一个脚接地,并联电容的大小为(CL-10)pF,,CL为晶振的负载电容大小,可通过晶振的datasheet中查到

    但是TMDSEVM6678中的那个并联电容是没有焊接的NL。而且他选择的晶振CL是20pF的?这个怎么解释?难道负载电容是20pF的电容如果一端接地后,负载电容就是1/2*CL?

      谢谢!

  • 个人认为TMDSEVM6678并联电容是预留的,如有需要的话还是需要并联上的,并非像你说的负载电容变为1/2.

  • EVM6678的板子上确实没有焊接,如果是这样的话,电容显然不匹配,为什么还能正常工作?一个是10pF ,另一个是20pF,这个怎么解释?

  • 是的,如果电容不匹配的话,晶振应该不会起振的,不能正常工作的, 你是用的EVM6678的EVM板? 如果是的话,建议到C6000 多核板块去咨询这个问题

  • 我们板子上用的也是6678,所以参考的EVM6678的开发板,实际上EVM6678板子可以正常工作,并没有因为CDCE62005的 AUX_IN是10pF,晶振是20pF的负载电容而出问题。