This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
如图所示,核心芯片采用AM5728,接口芯片采用TPD12S016,防护芯片采用TPD1E01B04DPYR,做静电测试,如果是+4kv,屏幕会重新启动,但是-4kv屏幕不重新启动,一直黑屏状态。如果将HDMI接口拔掉在重插,屏幕就会正常显示,请问哪里出了问题,电路图如图所示。PGND与GND之前采用的RC连接,R是1M,电容2.2nf/1kv,请帮忙分析下,谢谢
您好,谢谢您的回复;1.HDMi接口P11接的是屏幕,我们做静电时对机壳做静电,这个电路在板子上,板子在机壳上,如图所示对螺丝打静电,也对屏幕的螺丝打静电,对如图1处的螺丝打静电,正负4kv,2是连接屏幕的HDMI线,3是屏幕背面的螺丝,也要打静电,4是屏幕中有一个机壳地直接接到机壳上。经过测试,直接将屏幕放到贴颗上,将供电部分拿出来不在铁壳上,对1做静电也是出现屏幕黑暗情况.
2.PGND是机壳地,机壳地外接适配器直接可以和大地连接,经过测量与大地良好接触。
3.RC是并联的结构
确认下,下面截图中的两个电阻是不是没有接?因为在电路图中看不出对5V0有ESD防护。
在 HDMI 接口中与TPD12S016连接的信号网络中,如下截图信号都有满足±4KV的ESD防护,因此不太可能是TPD12S016 的问题。
因此,我建议您查下机壳内的电路板有哪些接口没有做ESD防护或者ESD防护等级不够。
我认为差分对之间不需要,每个接口对地都需要双向ESD管就可以了。将每个信号接口的±4KV静电泄放至地就可以了,因为地和机壳是连着的,而机壳是和大地连着的,这样静电就泄放至大地了。
对于HDMI接口的4个差分对您为什么不使用TPD12S016内部集成的 ESD 防护管?而又外接了8个TPD1E01B04?
因为静电是打在机壳上,而这个电路在板子上,板子在机壳上,所以请看看哪里还有静电通路到板子上?