This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
如图所示,核心芯片采用AM5728,接口芯片采用TPD12S016,防护芯片采用TPD1E01B04DPYR,做静电测试,如果是+4kv,屏幕会重新启动,但是-4kv屏幕不重新启动,一直黑屏状态。如果将HDMI接口拔掉在重插,屏幕就会正常显示,请问哪里出了问题,电路图如图所示。PGND与GND之前采用的RC连接,R是1M,电容2.2nf/1kv,请帮忙分析下,谢谢
您好,
静电测试时是将静电打在哪里?打在上电路图中哪个网络节点上?
PGND是指金属外壳吗?检查下PGND是否良好接大地?
PGND与GND之间是采用的RC串联还是并联连接?
您好,谢谢您的回复;1.HDMi接口P11接的是屏幕,我们做静电时对机壳做静电,这个电路在板子上,板子在机壳上,如图所示对螺丝打静电,也对屏幕的螺丝打静电,对如图1处的螺丝打静电,正负4kv,2是连接屏幕的HDMI线,3是屏幕背面的螺丝,也要打静电,4是屏幕中有一个机壳地直接接到机壳上。经过测试,直接将屏幕放到贴颗上,将供电部分拿出来不在铁壳上,对1做静电也是出现屏幕黑暗情况.
2.PGND是机壳地,机壳地外接适配器直接可以和大地连接,经过测量与大地良好接触。
3.RC是并联的结构