This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TI FAE你好:
我想请教一下关于PCA9534 和PCA9534A的问题。
这两个芯片的电源接法:PCA9534A在接入VCC的时候是不是一定要加一个100K的RES;PCA9534则不需要接电阻。
还有这两个芯片到底有什么区别因为第一次用这个芯片,PCA9534A VCC 没有接电阻,好像已经烧了几个,我只是TI的FAE确认一下
数据手册里是这样写的:
The PCA9534A and PCA9534 are identical, except for their fixed I2C address. This allows for up to 16 of thesedevices (8 of each) on the same I2C bus.
但是后面的Typical Application原理图上面两者VCC引脚相差一个100K的RES
VCC的最小值是2.3V,5V与VCC之间串接了100K之后,那么 ICC max = (5V-2.3V)/ 100K = 27uA,能驱动P0~P7么?
那数据手册肯定有问题了,这么一个简单的芯片我都调了2天了,IIC就是通信不上,程序应该没问题,因为我换一个其他设备的IIC地址都有ACK的
P0~P7全部空载,IIC也通信不上么?
是啊,我用的STM32,IIC用IO口模拟的,通信其他芯片没问题,难道速率也有规定?或者我IIC线没加电容?
是的,datasheet最后有给注释
是啊,我用的STM32,IIC用IO口模拟的------具体的型号?
F103ZET6,现在可以通讯上了,我也不知道为什么,可能跟两根线不一样长有关吧