Other Parts Discussed in Thread: PCA9534A, PCA9534
TI FAE你好:
我想请教一下关于PCA9534 和PCA9534A的问题。
这两个芯片的电源接法:PCA9534A在接入VCC的时候是不是一定要加一个100K的RES;PCA9534则不需要接电阻。
还有这两个芯片到底有什么区别
因为第一次用这个芯片,PCA9534A VCC 没有接电阻,好像已经烧了几个,我只是TI的FAE确认一下
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
那数据手册肯定有问题了,这么一个简单的芯片我都调了2天了,IIC就是通信不上,程序应该没问题,因为我换一个其他设备的IIC地址都有ACK的
是啊,我用的STM32,IIC用IO口模拟的,通信其他芯片没问题,难道速率也有规定?或者我IIC线没加电容?
F103ZET6,现在可以通讯上了,我也不知道为什么,可能跟两根线不一样长有关吧