This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
需求:FPGA出来的控制信号,需要将控制信号传输到单另外一个模块,传输线长度1.5m
问题:控制信号的传输逻辑电平使用LVDS还是LVPECL合适
如果使用SN65LVELT23做LVPECL转LVTTL,另外一个不用的通道,引脚直接悬空还是要上拉、接地?
谢谢!
LVDS相比LVPECL都是实现高速传输,LVDS属于电流驱动模式不容易产生开关尖峰,因而可以进一步降低噪音的影响 。这要看你实际需求咯,如果频率不是很高,用这两个没有太大性能差异。
谢谢。
The SN65LVELT23 is a low-power dual GND Ground
LVPECL/LVDS to LVTTL translator device.
The device includes circuitry to maintain inputs at VCC/2 when left open.
所以,悬空即可,对吧?