This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB913和914的配对使用问题



对于913来说,输入的信号为ITU656的8BIT数据,选择了D0-D7作为信号输入PIN,D8-D11悬空。

1、在和914配对使用时,8BIT的数据输出应该选择哪几个PIN?是D0-D7吗?

2、是否可以通过特定的寄存器来设定?

3、不用的PIN是否可OPEN处理?

希望TI工程师帮忙解答,谢谢