This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI experts,
We want to adjust the parameter configuration of DS80PCI800 chip under SMBUS SLAVE MODE,On the Repeater Page, we adjusted the parameter values of EQ CONTROL, DEM and VOD,Then click "APPLY TO ALL CHANNEL",But when I read the files in EEPROM, I found that the files in EEPROM did not change。
When I adjust the parameters under the EEPROM PAGE page, the files in the EEPROM also do not change. Please help me , how can I successfully write the configuration file I need into my EEPROM?
您好,选择Slot#0,然后右边选中0xB0这里可以吗?我估计您是下面步骤的第6步之类没有更新的原因。
按照下面的步骤再试试:
1. Start GUI
2. Click DS80PCI800 - Configuration Tab
3. Click "Apply" button on upper right of window
4. Use "Repeater Page" Tab to configure DS80PCI800
a. Select desired EQ/DEM/VOD settings - make sure to Click "Apply to Channel" or "Apply to All Channels" for each selection
5. Goto "EEPROM Page"
6. Click "Update Slot From Device
a. This will load the settings from the "Repeater Page" into the EEPROM Page
7. You should now see the updated EEPROM Data on the right side of page.
8 Click "Write to EEPROM Hex" to create file.
好的,我会重新尝试。按照您的步骤可以将写入的数据保持存到EEPROM中是吗;当前我是可以生产出对应的HEX文件的,只是将我的EEPROM中的内容读取出来时发现我的内容并未发生改变。
我的设备上是有4各DS80PCI800的芯片的,写入配置信息的方法也是相同的是吗
谢谢chen
好的,您这边试试,有任何问题及时反馈。
四片DS80PCI800的话,配置的方法是一样的,只是slot#0 对应0XB0,slot#1对应0XB2,slot#2对应0XB4,slot#3对应0XB6.
HI Chen,按照您的方法我是生成了对应的HEX文件。但是当我退出调试GUI,我将我设备上的用于给DS80PCI800使用的EEPROM芯片取下并读取其中的bin文件时,我发现我所读取出来的内容与我使用调试前EEPROM芯片中的内容是一样的,即我认为我新调试的参数并没有成功的写入到EEPROM芯片中,请问这可能是哪里出了问题吗?我能确定我的EEPROM芯片没有开启写保护功能。附件中我上传了我所生成的hex文件,如果方便的话,您可以帮忙看看我的文件。5725_0210_1756.hex
另一个问题,按照您所说的方法生成的hex文件,可以直接将其作为烧录文件使用烧录器烧入EEPROM中使用吗?
谢谢!
抱歉,回复晚了,是的,SigCon Architect不支持直接将配置文件写到EEPROM中。需要使用外部的EEPROM programmer 才能将配置文件写进去。
在DS125DF111EVM user‘s gudie中的5.3部分有介绍。
https://www.ti.com/lit/ug/snlu158a/snlu158a.pdf