This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB935-Q1: 咨询DS90UB935的有关问题

Part Number: DS90UB935-Q1

你好,咨询一下,DS90UB935是否可以用外部无源晶振驱动;

以及我这边需要clkout输出24M给sensor,那么我clkin应该输入多少,寄存器应该怎么配置

  • DS90UB935是否可以用外部无源晶振驱动;

     参考时钟接在deserialzier侧。 

    以及我这边需要clkout输出24M给sensor,那么我clkin应该输入多少,寄存器应该怎么配置

    CLKIN用在non-sync模式下。 CLK_OUT在non sync模式下是disable。

    CLK_OUT 是作为给sensor提供参考时钟的,计算方法可以参考数据手册7.4.1.5 Configuring CLK_OUT部分的介绍,如果您需要24Mhz的频率,配置如下:

    UB935的寄存器配置: Reg 0x06 = 0x41   M=1,HS_CLK_DIV=4
                                           Reg 0x07 = 0x2A转化为十进制为42. 
    然后根据CLK_OUT计算公式,FC为4Gbps,CLK_OUT=4Gbps*【1/(4*42)】=23.81Mhz约24Mhz。

  • 另外再问一下,935的寄存器是否由deserialzier侧定义

  • 要看您的应用主控和ser还是des接,主控如果和Des端接的话,那么935的寄存器是由Des侧定义。

x 出现错误。请重试或与管理员联系。