Part Number: DS90UB935-Q1
你好,咨询一下,DS90UB935是否可以用外部无源晶振驱动;
以及我这边需要clkout输出24M给sensor,那么我clkin应该输入多少,寄存器应该怎么配置
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB935-Q1
你好,咨询一下,DS90UB935是否可以用外部无源晶振驱动;
以及我这边需要clkout输出24M给sensor,那么我clkin应该输入多少,寄存器应该怎么配置
DS90UB935是否可以用外部无源晶振驱动;
参考时钟接在deserialzier侧。
以及我这边需要clkout输出24M给sensor,那么我clkin应该输入多少,寄存器应该怎么配置
CLKIN用在non-sync模式下。 CLK_OUT在non sync模式下是disable。
CLK_OUT 是作为给sensor提供参考时钟的,计算方法可以参考数据手册7.4.1.5 Configuring CLK_OUT部分的介绍,如果您需要24Mhz的频率,配置如下:
UB935的寄存器配置: Reg 0x06 = 0x41 M=1,HS_CLK_DIV=4
Reg 0x07 = 0x2A转化为十进制为42.
然后根据CLK_OUT计算公式,FC为4Gbps,CLK_OUT=4Gbps*【1/(4*42)】=23.81Mhz约24Mhz。

要看您的应用主控和ser还是des接,主控如果和Des端接的话,那么935的寄存器是由Des侧定义。