This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65LVCP408 差分接收无信号?

Other Parts Discussed in Thread: SN65LVCP408, TMDS141

使用TMDS141驱动 SN65LVCP408 ,做差分交叉开关,无输出信号?

TMDS141, (1pin,2Pin)有差分信号输入,600mv,

输出端(9pin,10pin)无输出信号.

TMDS141的9pin,10pin 连接到SN65LVCP408 的(5pin,6pin),SN65LVCP408 的VCC为3.2V,vbb为1.6V,

测量5pin和6pin之间的电阻为100欧,

测量5pin到VCC电阻为30K?

测量5pin到VBB电阻为32K?

TMDS141的测量结果为

1pin和2pin为100欧

1pin到VCC为50欧

 

 

,

  • 问题应该在TMDS141,SN65LVCP408上电后,默认对应的通道输出。请查一下TMDS141有没有输出?

  • 将TMDS141的9pin,10pin 接到另外一颗TMDS141的(1pin,2pin)能测到输出信号.,证明TMDS141工作正常的.

    对SN65LVCP408 差分电阻值测量 很疑惑? 正常值都是50欧,但SN65LVCP408 测试出来是30K?什么原因呢?

    因为这个原因,所以TMDS141的输出脚(9pin,和10pin)均不能被上拉到3V,测量只有0.5V?

    如果SN65LVCP408 的(5pin)外接一颗100欧电阻到VCC,可以测到100mv左右的差分信号?

    SN65LVCP408 上电后复位 通到对应关为

    0-0

    1-1

    2-2

    3-3

    4-4

    5-5

    6-6

    7-7

    通过IIC接口能正常读取SN65LVCP408 寄存器值和写入值.

    看SN65LVCP408 数据手册 差分输入回路有RBBDC电阻?是该电阻导致介绍不正确?

  • RBBDC只是限流保护,差分偏置电压1.6V

x 出现错误。请重试或与管理员联系。