This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB1210: 关于DP,DM和VBUS的一些疑问

Part Number: TUSB1210


您好,我在使用TUSB1210芯片时,有些疑问需要您解答一下

1.VBUS是否必须接?

在手册第50页,8.2.1.2.1章节提到如果不用VBUS,建议接地,但浮空也可以接受;

在手册第54页,9章节下提到TUSB1210并不严格要求VBUS;

在手册第54页,9.1章节提到VBUS通常接到连接器的VBUS。

那么:VBUS在什么情况下时必须接5V?

当不接VBUS时,DP和DM处于什么状态,是无法识别下游设备吗?如HUB或U盘之类?

当我使用电源管理时,USB连接器并非一直有5V,此时还能接到连接器的VBUS上吗?

1.DP和DM是否可交换pin?

手册第43页,7.5.29章节中提到的DP/DM交换是指什么?