This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
SOC: TDA2
LINUX: 4.19.73
用的是内核自带的 DP83TC811 驱动
root@dra7xx-evm:~# ifconfig eth0 down
root@dra7xx-evm:~# ifconfig eth0 up
[ 40.771447] net eth0: initializing cpsw version 1.15 (0)
[ 40.780418] dp83811_config_init
[ 40.801049] TI DP83TC811 48485000.mdio:00: attached PHY driver [TI DP83TC811] (mii_bus:phy_addr=48485000.mdio:00, irq=POLL)
[ 40.816432] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
root@dra7xx-evm:~# [ 48.082181] cpsw 48484000.ethernet eth0: Link is Up - 10Mbps/Half - flow control off
[ 48.090023] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
您好,
下面文档中有工作在100base-t1 slave mode 和 master mode 下的硬件和软件配置,您看下对您是否有帮助:
您好,为更加有效地解决您的问题,我已将您的问题发布在E2E英文技术论坛上,请资深的英文论坛工程师为您提供帮助。
我测试使用的是两块相同的板子,网口用一对双绞线连接,仅仅DP83TC811 主/从配置不同,一块主,另一块为从。
驱动是 TDA2 VSDK: PROCESSOR_SDK_VISION_03_08_00_00 中 linux kernel 4.19.73 自带,路径: drivers/net/phy/dp83tc811.c,源码如下:
// SPDX-License-Identifier: GPL-2.0 /* * Driver for the Texas Instruments DP83TC811 PHY * * Copyright (C) 2018 Texas Instruments Incorporated - http://www.ti.com/ * */ #include <linux/ethtool.h> #include <linux/etherdevice.h> #include <linux/kernel.h> #include <linux/mii.h> #include <linux/module.h> #include <linux/of.h> #include <linux/phy.h> #include <linux/netdevice.h> #define DP83TC811_PHY_ID 0x2000a253 #define DP83811_DEVADDR 0x1f #define MII_DP83811_SGMII_CTRL 0x09 #define MII_DP83811_INT_STAT1 0x12 #define MII_DP83811_INT_STAT2 0x13 #define MII_DP83811_INT_STAT3 0x18 #define MII_DP83811_RESET_CTRL 0x1f #define DP83811_HW_RESET BIT(15) #define DP83811_SW_RESET BIT(14) /* INT_STAT1 bits */ #define DP83811_RX_ERR_HF_INT_EN BIT(0) #define DP83811_MS_TRAINING_INT_EN BIT(1) #define DP83811_ANEG_COMPLETE_INT_EN BIT(2) #define DP83811_ESD_EVENT_INT_EN BIT(3) #define DP83811_WOL_INT_EN BIT(4) #define DP83811_LINK_STAT_INT_EN BIT(5) #define DP83811_ENERGY_DET_INT_EN BIT(6) #define DP83811_LINK_QUAL_INT_EN BIT(7) /* INT_STAT2 bits */ #define DP83811_JABBER_DET_INT_EN BIT(0) #define DP83811_POLARITY_INT_EN BIT(1) #define DP83811_SLEEP_MODE_INT_EN BIT(2) #define DP83811_OVERTEMP_INT_EN BIT(3) #define DP83811_OVERVOLTAGE_INT_EN BIT(6) #define DP83811_UNDERVOLTAGE_INT_EN BIT(7) /* INT_STAT3 bits */ #define DP83811_LPS_INT_EN BIT(0) #define DP83811_NO_FRAME_INT_EN BIT(3) #define DP83811_POR_DONE_INT_EN BIT(4) #define MII_DP83811_RXSOP1 0x04a5 #define MII_DP83811_RXSOP2 0x04a6 #define MII_DP83811_RXSOP3 0x04a7 /* WoL Registers */ #define MII_DP83811_WOL_CFG 0x04a0 #define MII_DP83811_WOL_STAT 0x04a1 #define MII_DP83811_WOL_DA1 0x04a2 #define MII_DP83811_WOL_DA2 0x04a3 #define MII_DP83811_WOL_DA3 0x04a4 /* WoL bits */ #define DP83811_WOL_MAGIC_EN BIT(0) #define DP83811_WOL_SECURE_ON BIT(5) #define DP83811_WOL_EN BIT(7) #define DP83811_WOL_INDICATION_SEL BIT(8) #define DP83811_WOL_CLR_INDICATION BIT(11) /* SGMII CTRL bits */ #define DP83811_TDR_AUTO BIT(8) #define DP83811_SGMII_EN BIT(12) #define DP83811_SGMII_AUTO_NEG_EN BIT(13) #define DP83811_SGMII_TX_ERR_DIS BIT(14) #define DP83811_SGMII_SOFT_RESET BIT(15) static int dp83811_ack_interrupt(struct phy_device *phydev) { int err; err = phy_read(phydev, MII_DP83811_INT_STAT1); if (err < 0) return err; err = phy_read(phydev, MII_DP83811_INT_STAT2); if (err < 0) return err; err = phy_read(phydev, MII_DP83811_INT_STAT3); if (err < 0) return err; return 0; } static int dp83811_set_wol(struct phy_device *phydev, struct ethtool_wolinfo *wol) { struct net_device *ndev = phydev->attached_dev; const u8 *mac; u16 value; if (wol->wolopts & (WAKE_MAGIC | WAKE_MAGICSECURE)) { mac = (const u8 *)ndev->dev_addr; if (!is_valid_ether_addr(mac)) return -EINVAL; /* MAC addresses start with byte 5, but stored in mac[0]. * 811 PHYs store bytes 4|5, 2|3, 0|1 */ phy_write_mmd(phydev, DP83811_DEVADDR, MII_DP83811_WOL_DA1, (mac[1] << 8) | mac[0]); phy_write_mmd(phydev, DP83811_DEVADDR, MII_DP83811_WOL_DA2, (mac[3] << 8) | mac[2]); phy_write_mmd(phydev, DP83811_DEVADDR, MII_DP83811_WOL_DA3, (mac[5] << 8) | mac[4]); value = phy_read_mmd(phydev, DP83811_DEVADDR, MII_DP83811_WOL_CFG); if (wol->wolopts & WAKE_MAGIC) value |= DP83811_WOL_MAGIC_EN; else value &= ~DP83811_WOL_MAGIC_EN; if (wol->wolopts & WAKE_MAGICSECURE) { phy_write_mmd(phydev, DP83811_DEVADDR, MII_DP83811_RXSOP1, (wol->sopass[1] << 8) | wol->sopass[0]); phy_write_mmd(phydev, DP83811_DEVADDR, MII_DP83811_RXSOP2, (wol->sopass[3] << 8) | wol->sopass[2]); phy_write_mmd(phydev, DP83811_DEVADDR, MII_DP83811_RXSOP3, (wol->sopass[5] << 8) | wol->sopass[4]); value |= DP83811_WOL_SECURE_ON; } else { value &= ~DP83811_WOL_SECURE_ON; } value |= (DP83811_WOL_EN | DP83811_WOL_INDICATION_SEL | DP83811_WOL_CLR_INDICATION); phy_write_mmd(phydev, DP83811_DEVADDR, MII_DP83811_WOL_CFG, value); } else { value = phy_read_mmd(phydev, DP83811_DEVADDR, MII_DP83811_WOL_CFG); value &= ~DP83811_WOL_EN; phy_write_mmd(phydev, DP83811_DEVADDR, MII_DP83811_WOL_CFG, value); } return 0; } static void dp83811_get_wol(struct phy_device *phydev, struct ethtool_wolinfo *wol) { u16 sopass_val; int value; wol->supported = (WAKE_MAGIC | WAKE_MAGICSECURE); wol->wolopts = 0; value = phy_read_mmd(phydev, DP83811_DEVADDR, MII_DP83811_WOL_CFG); if (value & DP83811_WOL_MAGIC_EN) wol->wolopts |= WAKE_MAGIC; if (value & DP83811_WOL_SECURE_ON) { sopass_val = phy_read_mmd(phydev, DP83811_DEVADDR, MII_DP83811_RXSOP1); wol->sopass[0] = (sopass_val & 0xff); wol->sopass[1] = (sopass_val >> 8); sopass_val = phy_read_mmd(phydev, DP83811_DEVADDR, MII_DP83811_RXSOP2); wol->sopass[2] = (sopass_val & 0xff); wol->sopass[3] = (sopass_val >> 8); sopass_val = phy_read_mmd(phydev, DP83811_DEVADDR, MII_DP83811_RXSOP3); wol->sopass[4] = (sopass_val & 0xff); wol->sopass[5] = (sopass_val >> 8); wol->wolopts |= WAKE_MAGICSECURE; } /* WoL is not enabled so set wolopts to 0 */ if (!(value & DP83811_WOL_EN)) wol->wolopts = 0; } static int dp83811_config_intr(struct phy_device *phydev) { int misr_status, err; if (phydev->interrupts == PHY_INTERRUPT_ENABLED) { misr_status = phy_read(phydev, MII_DP83811_INT_STAT1); if (misr_status < 0) return misr_status; misr_status |= (DP83811_RX_ERR_HF_INT_EN | DP83811_MS_TRAINING_INT_EN | DP83811_ANEG_COMPLETE_INT_EN | DP83811_ESD_EVENT_INT_EN | DP83811_WOL_INT_EN | DP83811_LINK_STAT_INT_EN | DP83811_ENERGY_DET_INT_EN | DP83811_LINK_QUAL_INT_EN); err = phy_write(phydev, MII_DP83811_INT_STAT1, misr_status); if (err < 0) return err; misr_status = phy_read(phydev, MII_DP83811_INT_STAT2); if (misr_status < 0) return misr_status; misr_status |= (DP83811_JABBER_DET_INT_EN | DP83811_POLARITY_INT_EN | DP83811_SLEEP_MODE_INT_EN | DP83811_OVERTEMP_INT_EN | DP83811_OVERVOLTAGE_INT_EN | DP83811_UNDERVOLTAGE_INT_EN); err = phy_write(phydev, MII_DP83811_INT_STAT2, misr_status); if (err < 0) return err; misr_status = phy_read(phydev, MII_DP83811_INT_STAT3); if (misr_status < 0) return misr_status; misr_status |= (DP83811_LPS_INT_EN | DP83811_NO_FRAME_INT_EN | DP83811_POR_DONE_INT_EN); err = phy_write(phydev, MII_DP83811_INT_STAT3, misr_status); } else { err = phy_write(phydev, MII_DP83811_INT_STAT1, 0); if (err < 0) return err; err = phy_write(phydev, MII_DP83811_INT_STAT2, 0); if (err < 0) return err; err = phy_write(phydev, MII_DP83811_INT_STAT3, 0); } return err; } static int dp83811_config_aneg(struct phy_device *phydev) { int value, err; if (phydev->interface == PHY_INTERFACE_MODE_SGMII) { value = phy_read(phydev, MII_DP83811_SGMII_CTRL); if (phydev->autoneg == AUTONEG_ENABLE) { err = phy_write(phydev, MII_DP83811_SGMII_CTRL, (DP83811_SGMII_AUTO_NEG_EN | value)); if (err < 0) return err; } else { err = phy_write(phydev, MII_DP83811_SGMII_CTRL, (~DP83811_SGMII_AUTO_NEG_EN & value)); if (err < 0) return err; } } return genphy_config_aneg(phydev); } static int dp83811_config_init(struct phy_device *phydev) { int value, err; err = genphy_config_init(phydev); if (err < 0) return err; value = phy_read(phydev, MII_DP83811_SGMII_CTRL); if (phydev->interface == PHY_INTERFACE_MODE_SGMII) { err = phy_write(phydev, MII_DP83811_SGMII_CTRL, (DP83811_SGMII_EN | value)); } else { err = phy_write(phydev, MII_DP83811_SGMII_CTRL, (~DP83811_SGMII_EN & value)); } if (err < 0) return err; value = DP83811_WOL_MAGIC_EN | DP83811_WOL_SECURE_ON | DP83811_WOL_EN; return phy_write_mmd(phydev, DP83811_DEVADDR, MII_DP83811_WOL_CFG, value); } static int dp83811_phy_reset(struct phy_device *phydev) { int err; err = phy_write(phydev, MII_DP83811_RESET_CTRL, DP83811_HW_RESET); if (err < 0) return err; return 0; } static int dp83811_suspend(struct phy_device *phydev) { int value; value = phy_read_mmd(phydev, DP83811_DEVADDR, MII_DP83811_WOL_CFG); if (!(value & DP83811_WOL_EN)) genphy_suspend(phydev); return 0; } static int dp83811_resume(struct phy_device *phydev) { int value; genphy_resume(phydev); value = phy_read_mmd(phydev, DP83811_DEVADDR, MII_DP83811_WOL_CFG); phy_write_mmd(phydev, DP83811_DEVADDR, MII_DP83811_WOL_CFG, value | DP83811_WOL_CLR_INDICATION); return 0; } static struct phy_driver dp83811_driver[] = { { .phy_id = DP83TC811_PHY_ID, .phy_id_mask = 0xfffffff0, .name = "TI DP83TC811", .features = PHY_BASIC_FEATURES, .flags = PHY_HAS_INTERRUPT, .config_init = dp83811_config_init, .config_aneg = dp83811_config_aneg, .soft_reset = dp83811_phy_reset, .get_wol = dp83811_get_wol, .set_wol = dp83811_set_wol, .ack_interrupt = dp83811_ack_interrupt, .config_intr = dp83811_config_intr, .suspend = dp83811_suspend, .resume = dp83811_resume, }, }; module_phy_driver(dp83811_driver); static struct mdio_device_id __maybe_unused dp83811_tbl[] = { { DP83TC811_PHY_ID, 0xfffffff0 }, { }, }; MODULE_DEVICE_TABLE(mdio, dp83811_tbl); MODULE_DESCRIPTION("Texas Instruments DP83TC811 PHY driver"); MODULE_AUTHOR("Dan Murphy <dmurphy@ti.com"); MODULE_LICENSE("GPL");