This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83TC811R-Q1: 工作在 10Mbps/Half 而不是 100Mbps,如何排查调试? 麻烦给点思路

Part Number: DP83TC811R-Q1

SOC: TDA2

LINUX:  4.19.73 

用的是内核自带的 DP83TC811 驱动

root@dra7xx-evm:~# ifconfig eth0 down
root@dra7xx-evm:~# ifconfig eth0 up
[ 40.771447] net eth0: initializing cpsw version 1.15 (0)
[ 40.780418] dp83811_config_init
[ 40.801049] TI DP83TC811 48485000.mdio:00: attached PHY driver [TI DP83TC811] (mii_bus:phy_addr=48485000.mdio:00, irq=POLL)
[ 40.816432] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
root@dra7xx-evm:~# [ 48.082181] cpsw 48484000.ethernet eth0: Link is Up - 10Mbps/Half - flow control off
[ 48.090023] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready

  • 您好,

    下面文档中有工作在100base-t1 slave mode 和 master mode 下的硬件和软件配置,您看下对您是否有帮助:

    https://www.ti.com/lit/an/snla293/snla293.pdf

  • 对于该文档列出的寄存器和值,我在驱动文件的dp83811_config_init 函数中依次调用phy_write_mmd 写入,问题依旧。(我随后调用 phy_read_mmd读出,对比确定值写入的没有问题) 还有什么排查手段吗?

  • 您好,为更加有效地解决您的问题,我已将您的问题发布在E2E英文技术论坛上,请资深的英文论坛工程师为您提供帮助。

    英文论坛对应子论坛链接:https://e2e.ti.com/support/interface-group/interface/f/interface-forum/1202586/dp83tc811r-q1-working-at-10mbps-half-instead-of-100mbps

  • 别客气~

    由于时差问题,他们应该今天晚上会给回复,请耐心等下

  • 正在使用哪个link partner?您可以尝试连接其他link partner 吗?

    还请分享使用的驱动程序。

    What link partner is being used? Can you try connecting a different link partner?

    Please also share the driver which was used.

  • 我测试使用的是两块相同的板子,网口用一对双绞线连接,仅仅DP83TC811 主/从配置不同,一块主,另一块为从。

    驱动是 TDA2 VSDK: PROCESSOR_SDK_VISION_03_08_00_00 中 linux kernel  4.19.73  自带,路径: drivers/net/phy/dp83tc811.c,源码如下:

    // SPDX-License-Identifier: GPL-2.0
    /*
     * Driver for the Texas Instruments DP83TC811 PHY
     *
     * Copyright (C) 2018 Texas Instruments Incorporated - http://www.ti.com/
     *
     */
    
    #include <linux/ethtool.h>
    #include <linux/etherdevice.h>
    #include <linux/kernel.h>
    #include <linux/mii.h>
    #include <linux/module.h>
    #include <linux/of.h>
    #include <linux/phy.h>
    #include <linux/netdevice.h>
    
    #define DP83TC811_PHY_ID	0x2000a253
    #define DP83811_DEVADDR		0x1f
    
    #define MII_DP83811_SGMII_CTRL	0x09
    #define MII_DP83811_INT_STAT1	0x12
    #define MII_DP83811_INT_STAT2	0x13
    #define MII_DP83811_INT_STAT3	0x18
    #define MII_DP83811_RESET_CTRL	0x1f
    
    #define DP83811_HW_RESET	BIT(15)
    #define DP83811_SW_RESET	BIT(14)
    
    /* INT_STAT1 bits */
    #define DP83811_RX_ERR_HF_INT_EN	BIT(0)
    #define DP83811_MS_TRAINING_INT_EN	BIT(1)
    #define DP83811_ANEG_COMPLETE_INT_EN	BIT(2)
    #define DP83811_ESD_EVENT_INT_EN	BIT(3)
    #define DP83811_WOL_INT_EN		BIT(4)
    #define DP83811_LINK_STAT_INT_EN	BIT(5)
    #define DP83811_ENERGY_DET_INT_EN	BIT(6)
    #define DP83811_LINK_QUAL_INT_EN	BIT(7)
    
    /* INT_STAT2 bits */
    #define DP83811_JABBER_DET_INT_EN	BIT(0)
    #define DP83811_POLARITY_INT_EN		BIT(1)
    #define DP83811_SLEEP_MODE_INT_EN	BIT(2)
    #define DP83811_OVERTEMP_INT_EN		BIT(3)
    #define DP83811_OVERVOLTAGE_INT_EN	BIT(6)
    #define DP83811_UNDERVOLTAGE_INT_EN	BIT(7)
    
    /* INT_STAT3 bits */
    #define DP83811_LPS_INT_EN	BIT(0)
    #define DP83811_NO_FRAME_INT_EN	BIT(3)
    #define DP83811_POR_DONE_INT_EN	BIT(4)
    
    #define MII_DP83811_RXSOP1	0x04a5
    #define MII_DP83811_RXSOP2	0x04a6
    #define MII_DP83811_RXSOP3	0x04a7
    
    /* WoL Registers */
    #define MII_DP83811_WOL_CFG	0x04a0
    #define MII_DP83811_WOL_STAT	0x04a1
    #define MII_DP83811_WOL_DA1	0x04a2
    #define MII_DP83811_WOL_DA2	0x04a3
    #define MII_DP83811_WOL_DA3	0x04a4
    
    /* WoL bits */
    #define DP83811_WOL_MAGIC_EN	BIT(0)
    #define DP83811_WOL_SECURE_ON	BIT(5)
    #define DP83811_WOL_EN		BIT(7)
    #define DP83811_WOL_INDICATION_SEL BIT(8)
    #define DP83811_WOL_CLR_INDICATION BIT(11)
    
    /* SGMII CTRL bits */
    #define DP83811_TDR_AUTO		BIT(8)
    #define DP83811_SGMII_EN		BIT(12)
    #define DP83811_SGMII_AUTO_NEG_EN	BIT(13)
    #define DP83811_SGMII_TX_ERR_DIS	BIT(14)
    #define DP83811_SGMII_SOFT_RESET	BIT(15)
    
    static int dp83811_ack_interrupt(struct phy_device *phydev)
    {
    	int err;
    
    	err = phy_read(phydev, MII_DP83811_INT_STAT1);
    	if (err < 0)
    		return err;
    
    	err = phy_read(phydev, MII_DP83811_INT_STAT2);
    	if (err < 0)
    		return err;
    
    	err = phy_read(phydev, MII_DP83811_INT_STAT3);
    	if (err < 0)
    		return err;
    
    	return 0;
    }
    
    static int dp83811_set_wol(struct phy_device *phydev,
    			   struct ethtool_wolinfo *wol)
    {
    	struct net_device *ndev = phydev->attached_dev;
    	const u8 *mac;
    	u16 value;
    
    	if (wol->wolopts & (WAKE_MAGIC | WAKE_MAGICSECURE)) {
    		mac = (const u8 *)ndev->dev_addr;
    
    		if (!is_valid_ether_addr(mac))
    			return -EINVAL;
    
    		/* MAC addresses start with byte 5, but stored in mac[0].
    		 * 811 PHYs store bytes 4|5, 2|3, 0|1
    		 */
    		phy_write_mmd(phydev, DP83811_DEVADDR, MII_DP83811_WOL_DA1,
    			      (mac[1] << 8) | mac[0]);
    		phy_write_mmd(phydev, DP83811_DEVADDR, MII_DP83811_WOL_DA2,
    			      (mac[3] << 8) | mac[2]);
    		phy_write_mmd(phydev, DP83811_DEVADDR, MII_DP83811_WOL_DA3,
    			      (mac[5] << 8) | mac[4]);
    
    		value = phy_read_mmd(phydev, DP83811_DEVADDR,
    				     MII_DP83811_WOL_CFG);
    		if (wol->wolopts & WAKE_MAGIC)
    			value |= DP83811_WOL_MAGIC_EN;
    		else
    			value &= ~DP83811_WOL_MAGIC_EN;
    
    		if (wol->wolopts & WAKE_MAGICSECURE) {
    			phy_write_mmd(phydev, DP83811_DEVADDR,
    				      MII_DP83811_RXSOP1,
    				      (wol->sopass[1] << 8) | wol->sopass[0]);
    			phy_write_mmd(phydev, DP83811_DEVADDR,
    				      MII_DP83811_RXSOP2,
    				      (wol->sopass[3] << 8) | wol->sopass[2]);
    			phy_write_mmd(phydev, DP83811_DEVADDR,
    				      MII_DP83811_RXSOP3,
    				      (wol->sopass[5] << 8) | wol->sopass[4]);
    			value |= DP83811_WOL_SECURE_ON;
    		} else {
    			value &= ~DP83811_WOL_SECURE_ON;
    		}
    
    		value |= (DP83811_WOL_EN | DP83811_WOL_INDICATION_SEL |
    			  DP83811_WOL_CLR_INDICATION);
    		phy_write_mmd(phydev, DP83811_DEVADDR, MII_DP83811_WOL_CFG,
    			      value);
    	} else {
    		value = phy_read_mmd(phydev, DP83811_DEVADDR,
    				     MII_DP83811_WOL_CFG);
    		value &= ~DP83811_WOL_EN;
    		phy_write_mmd(phydev, DP83811_DEVADDR, MII_DP83811_WOL_CFG,
    			      value);
    	}
    
    	return 0;
    }
    
    static void dp83811_get_wol(struct phy_device *phydev,
    			    struct ethtool_wolinfo *wol)
    {
    	u16 sopass_val;
    	int value;
    
    	wol->supported = (WAKE_MAGIC | WAKE_MAGICSECURE);
    	wol->wolopts = 0;
    
    	value = phy_read_mmd(phydev, DP83811_DEVADDR, MII_DP83811_WOL_CFG);
    
    	if (value & DP83811_WOL_MAGIC_EN)
    		wol->wolopts |= WAKE_MAGIC;
    
    	if (value & DP83811_WOL_SECURE_ON) {
    		sopass_val = phy_read_mmd(phydev, DP83811_DEVADDR,
    					  MII_DP83811_RXSOP1);
    		wol->sopass[0] = (sopass_val & 0xff);
    		wol->sopass[1] = (sopass_val >> 8);
    
    		sopass_val = phy_read_mmd(phydev, DP83811_DEVADDR,
    					  MII_DP83811_RXSOP2);
    		wol->sopass[2] = (sopass_val & 0xff);
    		wol->sopass[3] = (sopass_val >> 8);
    
    		sopass_val = phy_read_mmd(phydev, DP83811_DEVADDR,
    					  MII_DP83811_RXSOP3);
    		wol->sopass[4] = (sopass_val & 0xff);
    		wol->sopass[5] = (sopass_val >> 8);
    
    		wol->wolopts |= WAKE_MAGICSECURE;
    	}
    
    	/* WoL is not enabled so set wolopts to 0 */
    	if (!(value & DP83811_WOL_EN))
    		wol->wolopts = 0;
    }
    
    static int dp83811_config_intr(struct phy_device *phydev)
    {
    	int misr_status, err;
    
    	if (phydev->interrupts == PHY_INTERRUPT_ENABLED) {
    		misr_status = phy_read(phydev, MII_DP83811_INT_STAT1);
    		if (misr_status < 0)
    			return misr_status;
    
    		misr_status |= (DP83811_RX_ERR_HF_INT_EN |
    				DP83811_MS_TRAINING_INT_EN |
    				DP83811_ANEG_COMPLETE_INT_EN |
    				DP83811_ESD_EVENT_INT_EN |
    				DP83811_WOL_INT_EN |
    				DP83811_LINK_STAT_INT_EN |
    				DP83811_ENERGY_DET_INT_EN |
    				DP83811_LINK_QUAL_INT_EN);
    
    		err = phy_write(phydev, MII_DP83811_INT_STAT1, misr_status);
    		if (err < 0)
    			return err;
    
    		misr_status = phy_read(phydev, MII_DP83811_INT_STAT2);
    		if (misr_status < 0)
    			return misr_status;
    
    		misr_status |= (DP83811_JABBER_DET_INT_EN |
    				DP83811_POLARITY_INT_EN |
    				DP83811_SLEEP_MODE_INT_EN |
    				DP83811_OVERTEMP_INT_EN |
    				DP83811_OVERVOLTAGE_INT_EN |
    				DP83811_UNDERVOLTAGE_INT_EN);
    
    		err = phy_write(phydev, MII_DP83811_INT_STAT2, misr_status);
    		if (err < 0)
    			return err;
    
    		misr_status = phy_read(phydev, MII_DP83811_INT_STAT3);
    		if (misr_status < 0)
    			return misr_status;
    
    		misr_status |= (DP83811_LPS_INT_EN |
    				DP83811_NO_FRAME_INT_EN |
    				DP83811_POR_DONE_INT_EN);
    
    		err = phy_write(phydev, MII_DP83811_INT_STAT3, misr_status);
    
    	} else {
    		err = phy_write(phydev, MII_DP83811_INT_STAT1, 0);
    		if (err < 0)
    			return err;
    
    		err = phy_write(phydev, MII_DP83811_INT_STAT2, 0);
    		if (err < 0)
    			return err;
    
    		err = phy_write(phydev, MII_DP83811_INT_STAT3, 0);
    	}
    
    	return err;
    }
    
    static int dp83811_config_aneg(struct phy_device *phydev)
    {
    	int value, err;
    
    	if (phydev->interface == PHY_INTERFACE_MODE_SGMII) {
    		value = phy_read(phydev, MII_DP83811_SGMII_CTRL);
    		if (phydev->autoneg == AUTONEG_ENABLE) {
    			err = phy_write(phydev, MII_DP83811_SGMII_CTRL,
    					(DP83811_SGMII_AUTO_NEG_EN | value));
    			if (err < 0)
    				return err;
    		} else {
    			err = phy_write(phydev, MII_DP83811_SGMII_CTRL,
    					(~DP83811_SGMII_AUTO_NEG_EN & value));
    			if (err < 0)
    				return err;
    		}
    	}
    
    	return genphy_config_aneg(phydev);
    }
    
    static int dp83811_config_init(struct phy_device *phydev)
    {
    	int value, err;
    
    	err = genphy_config_init(phydev);
    	if (err < 0)
    		return err;
    
    	value = phy_read(phydev, MII_DP83811_SGMII_CTRL);
    	if (phydev->interface == PHY_INTERFACE_MODE_SGMII) {
    		err = phy_write(phydev, MII_DP83811_SGMII_CTRL,
    					(DP83811_SGMII_EN | value));
    	} else {
    		err = phy_write(phydev, MII_DP83811_SGMII_CTRL,
    				(~DP83811_SGMII_EN & value));
    	}
    
    	if (err < 0)
    
    		return err;
    
    	value = DP83811_WOL_MAGIC_EN | DP83811_WOL_SECURE_ON | DP83811_WOL_EN;
    
    	return phy_write_mmd(phydev, DP83811_DEVADDR, MII_DP83811_WOL_CFG,
    	      value);
    }
    
    static int dp83811_phy_reset(struct phy_device *phydev)
    {
    	int err;
    
    	err = phy_write(phydev, MII_DP83811_RESET_CTRL, DP83811_HW_RESET);
    	if (err < 0)
    		return err;
    
    	return 0;
    }
    
    static int dp83811_suspend(struct phy_device *phydev)
    {
    	int value;
    
    	value = phy_read_mmd(phydev, DP83811_DEVADDR, MII_DP83811_WOL_CFG);
    
    	if (!(value & DP83811_WOL_EN))
    		genphy_suspend(phydev);
    
    	return 0;
    }
    
    static int dp83811_resume(struct phy_device *phydev)
    {
    	int value;
    
    	genphy_resume(phydev);
    
    	value = phy_read_mmd(phydev, DP83811_DEVADDR, MII_DP83811_WOL_CFG);
    
    	phy_write_mmd(phydev, DP83811_DEVADDR, MII_DP83811_WOL_CFG, value |
    		      DP83811_WOL_CLR_INDICATION);
    
    	return 0;
    }
    
    static struct phy_driver dp83811_driver[] = {
    	{
    		.phy_id = DP83TC811_PHY_ID,
    		.phy_id_mask = 0xfffffff0,
    		.name = "TI DP83TC811",
    		.features = PHY_BASIC_FEATURES,
    		.flags = PHY_HAS_INTERRUPT,
    		.config_init = dp83811_config_init,
    		.config_aneg = dp83811_config_aneg,
    		.soft_reset = dp83811_phy_reset,
    		.get_wol = dp83811_get_wol,
    		.set_wol = dp83811_set_wol,
    		.ack_interrupt = dp83811_ack_interrupt,
    		.config_intr = dp83811_config_intr,
    		.suspend = dp83811_suspend,
    		.resume = dp83811_resume,
    	 },
    };
    module_phy_driver(dp83811_driver);
    
    static struct mdio_device_id __maybe_unused dp83811_tbl[] = {
    	{ DP83TC811_PHY_ID, 0xfffffff0 },
    	{ },
    };
    MODULE_DEVICE_TABLE(mdio, dp83811_tbl);
    
    MODULE_DESCRIPTION("Texas Instruments DP83TC811 PHY driver");
    MODULE_AUTHOR("Dan Murphy <dmurphy@ti.com");
    MODULE_LICENSE("GPL");
    

  • 已将上述信息回复给美国的工程师,请耐心等待他们的答复。

  • 您使用的MAC接口是什么?

  • 您的问题是否已经解决,如果还没有解决,请反馈以上信息