Part Number: TUSB542


你好,这个芯片的的配置引脚有什么用,按图中的方式全部下拉可以吗,现在我SEL为低的情况下,通道二怎么不通呢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,SEL用来控制Host端和device端哪路是导通的。

可以看到当SEL为低时,TX_CON2和RX_CON2都是接GND的,TX_CON1和RX_CON1分别时和Host端的TX_AP和RX_AP连接的。

关于其他的几个配置引脚的高低电平,CNFG_A1和CNFG_B1是控制host端和TUSB542的预加重DE,均衡EQ以及输出幅值OS的处理,而
CNFG_A2和CNFG_B2则是对TUSB542和sink端的预加重DE,均衡EQ以及输出幅值OS的处理。

当SEL为低时TX_CON2和RX_CON2是和TX_AP和RX_AP连接的吧
是的,不好意思上面我写错了,SEL=L,TX_CON2和RX_CON2是和TX_AP和RX_AP连接的,TX_CON1和RX_CON1接地。
您现在是怎么配置的?SEL=L,channel2不通是吗?SEL=H可以吗?