This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
DS110DF410目前在10.3125G速率下外接光模块使用正常,如果输入数据的速率换成了1.25G,输出对接1.25G的光模块,寄存器需要如何配置?
您好,0X2F bit7:4是配置data rate的,1.25G和3.125Gbps的寄存器配置是相同的,所以不需要更改寄存器的配置,参考Table2各种标准下的速率配置。
它举例10.3125Gbps和1.25Gbps 的data rate下 0x2F bit7:4都配置为0000.分频系数Divider以及VCO 粗调都是自动调节的。
也就是说,在不同的data rate下,VCO频率相同,divider会自动配置,0x2F配置的就是同一个值就能达到不同的速率。
但是如果VCO频率不相同,就无法自动去调节了,就需要更改寄存器。
您好:
我们这边按照默认的设置测出来现象是接上1.25G光模块后对接交换机后交换机能够显示LINK,但是数据无法ping通,不知道还有什么方式可以排查?
我们这边按照默认的设置测出来现象是接上1.25G光模块后对接交换机后交换机能够显示LINK
按照datasheet中的介绍,0x2F[7:4] = 0x6会自动切换10.3125Gbps和1.25Gbps两种速率。您的0x2F配置的是什么值,默认bit7:4=0000,并不是0110呢。
如果配置bit7:4=0110,1.25Gbps还不可以的话,建议按照下面寄存器的顺序,配置PPM count group 0 =10G(寄存器 0x60, 0x61)PPM count group 1=10.3125Gbps( registers 0x62, 0x63).
你好:
我们这边不做任何配置,两台设备(Device1和Device2)可以正常通讯,但是对接其他设备比如交换机无法通讯,请问下经过DS110DF410芯片后的数据是否有做了什么处理?比如有增加了什么协议在里面?
请问下经过DS110DF410芯片后的数据是否有做了什么处理?比如有增加了什么协议在里面?
仅仅是一款retimer,没有增加新的协议在里面,只是说这款retimer支持哪些协议,比如它支持10GbE 和1GbE应用,支持Front Port SFF 8431 (SFP+) Optical等应用。