lmk048xx的数据手册中未提供输入参考时钟为cml电平的参考电路,能否提供一份,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
参考电路, 可以看一下官方网站的
你指的CLKIN/CLKIN*输入吗?根据datasheet Page11的电气特性来看,并非标准CML电平,CML电平的Voh=1.9V,Vol=1.1V,Vcm=1.5V,而CLKin0/0* 和 CLKin1/1*的输入,datasheet中已经给出为0.5V~3.1Vpp,如果采用单端输入的话,是0.25V~2.4Vpp范围。你是想采用差分输入还是单端输入?user's guide中的电路确实看起来比较乱,找不到CLKin0/0* 和 CLKin1/1*是通过哪款时钟发生器产生的,SMA也看不出连接到哪里,应该是采用的时钟发生器这类仪器直接输出提供给lmk048xx作为时钟源,我再看看。
这个是LMK048xx器件datasheet中给出的CLKIN/CLKIN*电平的标准,Voh=2.4V,Vol=0.4V,那么共模电压为(2.4+0.4)/2=1.4V.