This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB941AS-Q1: DS90UB926Q, link lock, PCLK/DE/HS输出正常,VS输出一直低,显示黑屏

Part Number: DS90UB941AS-Q1


Hi,

          我们在调试DS90UB941as—DS90UB926q时,pclk输入正常,941和926 link lock,但是没有图像输出,

示波器量926输出的PCLK, DE, VS, HS信号,PCLK、DE、HS信号正常,VS信号一直为低。

 

          SOC(8155)----DSI1--->941----link1--->926,

          Display timing如下,DSI使用NonBurst_VSPulse输出。PCLK测量为31.5MHz,DE/HS信号在31.5KHz,VS信号一直为低。

          我看941的使用手册,根据《4.6 Configuration of Sync Width for Event Mode/Burst Mode》理解,

         在NonBurst_VSPulse,VS是根据DSI输入的VSS, VSE, HSS, HSE产生的。

          在Event和Burst,VS是根据DSI输入的VSS,HSS产生的。

 

          想请问下,这种没有VS信号输出,是941配置没配对,还是因为SOC DSI输出的VS, HS信号有缺失造成的?

 

          uVisWidth                              = '854'

          uHsyncFrontPorch               = '68'

          uHsyncWidth                        = '6'

          uHsyncBackPorch                 = '72'

          uVisHeight                             = '480'

          uVsyncFrontPorch                = '35'

          uVsyncWidth                         = '1'

          uVsyncBackPorch                 = '9'

          uPixelFreqInHz                      = '31500000'