This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
我们在调试DS90UB941as—DS90UB926q时,pclk输入正常,941和926 link lock,但是没有图像输出,
示波器量926输出的PCLK, DE, VS, HS信号,PCLK、DE、HS信号正常,VS信号一直为低。
SOC(8155)----DSI1--->941----link1--->926,
Display timing如下,DSI使用NonBurst_VSPulse输出。PCLK测量为31.5MHz,DE/HS信号在31.5KHz,VS信号一直为低。
我看941的使用手册,根据《4.6 Configuration of Sync Width for Event Mode/Burst Mode》理解,
在NonBurst_VSPulse,VS是根据DSI输入的VSS, VSE, HSS, HSE产生的。
在Event和Burst,VS是根据DSI输入的VSS,HSS产生的。
想请问下,这种没有VS信号输出,是941配置没配对,还是因为SOC DSI输出的VS, HS信号有缺失造成的?
uVisWidth = '854'
uHsyncFrontPorch = '68'
uHsyncWidth = '6'
uHsyncBackPorch = '72'
uVisHeight = '480'
uVsyncFrontPorch = '35'
uVsyncWidth = '1'
uVsyncBackPorch = '9'
uPixelFreqInHz = '31500000'
我们941的寄存器配置如下:
0x01, 0x02
0x01, 0x08
0x1e, 0x02
0x03, 0x8a
0x4f, 0x8c
0x5b, 0x00
0x56, 0x00
0x40, 0x08
0x41, 0x05
0x42, 0x00
0x40, 0x08
0x41, 0x20
0x42, 0x7f
0x40, 0x08
0x41, 0x21
0x42, 0x00
0x40, 0x10
0x41, 0x86
0x42, 0x0a
0x41, 0x94
0x42, 0x0a
0x01, 0x00
0x1e, 0x04
0x1E, 0x05
0x0E, 0x05
0xC6, 0x21
0x1E, 0x04
0x07, 0x94
0x08, 0x94
0x6C, 0x61
0xC2, 0x00
0x30, 0x01
为更加有效地解决您的问题,我已将您的问题发布在E2E英文技术论坛上,请更了解这款芯片的TI资深工程师为您解答,一旦得到回复后我会立即回复给您。帖子链接如下,您也可以关注帖子,以方便查看或追问后续疑问。