Other Parts Discussed in Thread: LMH0341, LMH0340
您好,LMH0341和LVDS0340的LVDS接口信号是支持2.5V还是3.3V标准?LVDS信号连接到FPGA的话,FPGA的VCCO电压用2.5V还是3.3V?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这个芯片有VDD2V5和VDD3V3中供电管脚,但是没有说明这两种电压是和电压还是IO电压,是那部分的IO电压,虽然写了是在VDD=3.3V条件下测试的,是否理解为他的IO电压就是3.3V?VDD3V3就是LVDS接口的接口电平?
lvds的标准电平是2.5V,接到FPGA的那个BANK的电压肯定得是2.5V
还没有,还在调试0341的方案,再过几天还是搞不定就换这个方案!建议你:一,先把0341给的官方程序看看,要是你觉得这个能够搞定那就没问题,其实官方的程序对应的开发板功能很强大,这样就导致里面很多东西用不着,然后我就看不懂了。你要是FPGA很牛逼,那就可以;二,GS2971集成了均衡器,不用单独接均衡器了,而且2971解码出来直接是YCrCb 4:2:2的信号,再做处理很方便。
好的,多谢linhua,多谢各位的指点了,为了安全器件,我还是把VCCO的电压做成可配置为3.3V和2.5V的吧。
好的,多谢linhua和各位的指点了。我还是将接口电压做成2.5V和3.3V可配置的吧。
如果指的是LVDS 接口电平,那么LVDS是低压差分信号,IO口的电平Voh=1.4V,Vol=1V,400mVpp。因此严格来说,3.3V或2.5V都不行,因为3.3V的Vih(min)=2V,Vil(max)=0.8V,2.5V CMOS的Vih(min)=1.7V,Vol(max)=0.7V,所以应该配置为1.8V 才比较确切。
Peter Zhang:
这个芯片有VDD2V5和VDD3V3中供电管脚,但是没有说明这两种电压是和电压还是IO电压,是那部分的IO电压,虽然写了是在VDD=3.3V条件下测试的,是否理解��他的IO电压就是3.3V?VDD3V3就是LVDS接口的接口电平?
Kailyn多谢您的解答,我打算将接口电压做成可配置的。非常感谢了。
您好, 请问LMH0341工作需要初始化哪些寄存器呢?? 有没有官方的demo可以参考呢
寄存器在默认配置下应该也能工作,只是为了某些应用需求去配置寄存器。
这款器件没有官方demo可参考呢。