This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

lmh0030怎么进入test模式

使用单片机对其进行控制字写入,逻辑为

触发aclk 3次(控制字的命令时钟较慢,不到1M,应该识别没有问题,为了保险此处触发aclk6次)

对多功能io口进行功能设置

format寄存器写入1a,即1080p25

video info0寄存器写入20 使能vpg filter

test mode0寄存器写入36,(datasheet上说这应该是normally on 的设置)

test0写入34这是对输出模式的选择

然后把io bit7置1,使能tpg enable

然后几毫秒后对vclk加入74.25MHz的时钟

请问这样设置有什么问题吗,pass/~fail管脚一直没有输出高电平,说明没有进入test模式。(当然我每个寄存器写入时都是按时序来的,就是ad[9:8]00地址,触发一次aclk,ad[9:8]11数据,触发一次aclk。写入IO口的数据也是只要触发一次aclk就可以了吧。以上命令都是以us级的速度写入的,应该可以读取吧。)请问一下各位专家,我这样设置为什么进入不了test模式呢?

会不会是format0,test mode0的设置有所多余,或者其他edh、anc寄存器有需要设置的没有设置?

还是时钟加的有问题,datasheet上特别说明最好写完命令再加时钟,我延时了几ms,还有datasheet上提到了使用默认的标清模式时vclk不可超过27MHz,否则锁相环会locking up,这和我对数模式的设置有关吧,比如我输出高清信号是不是要加74.25MHz的vclk?还是说仍需要27MHz的?

菜鸟学生求教