This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LVDS系列(DS90UB925Q\927Q\928Q)支持展频技术吗



大家好,想请教TI工程师一个问题

目前方案中,采用DS90UB925Q和DS90UB928Q配对传输视频信号,PCLK为51.2M 在EMC测试CE电流法项目中,102.4M超标严重,为51.2M倍频。因此想尝试用展频来降低102.4M的辐射。

请教下TI工程师

1、LVDS系列(DS90UB925Q\927Q\928Q)支持展频技术吗?

2、使用展频技术会有什么不良的后果?

  • 您好,

    Ux925/926支持SSC(展频), 而UX927/908不支持SSC.

    SSC在FPD-LINK2/3产品中的目的是为了减小TTL信号(host和发送端、接收端和host)的EMI问题。 而UX907/908支持LVDS差分信号,所以不需要SSC。

    关于SSC的使用请查阅Ux925/926的规格书, 后者有这更为详细的说明

    展频技术的目的就是为了降低EMI问题,只要在要求以内没有什么问题。

  • 你好,

    请问你的视频传输,是分为两个模块吗? EMI问题是在925板上还是在928板上?

    925 PCLK支持SSC input, 但是扩频功能需要在host 上实现。

    "

    Input SSC Tolerance (SSCT)
    The DS90UB925Q serializer is capable of tracking a triangular input spread spectrum clocking (SSC) profile up
    to +/-2.5% amplitude deviations (center spread), up to 35 kHz modulation at 5–85 MHz, from a host source.

    扩频后当然会增加频偏和jitter,但是只要在serdes的手册允许的范围内是可以的,其EMI有1改善。

     此外一般PCLK的二次谐波很少会泄露,是不是layout的问题?

    附件是FPD link III serdes layout设计指导,希望对你有帮助。

    regards,

    Ivan

    "

    Board layout and design for EMI EMC_for Customer.pdf
  • 谢谢解答,EMI问题初步判定在925板上,PCLK由HOST提供给925的,因此想确认925是否支持

  • 明白了,谢谢