Part Number: TVP5151
我使用STM32单片机控制TVP5151芯片时,发现STM32无法将TVP5151芯片的REST管脚拉低。STM32控制TVP5151 REST管脚拉低时该管脚上存在2.2V左右的电压,但未接入TVP5151芯片时STM32单片机自身管脚时可以拉低的。TVP5151芯片供电正常,各管脚无短路。请问这是什么问题呢?
电路图是参考TVP5151手册绘制的。tvp5151原理图.pdf
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TVP5151
我使用STM32单片机控制TVP5151芯片时,发现STM32无法将TVP5151芯片的REST管脚拉低。STM32控制TVP5151 REST管脚拉低时该管脚上存在2.2V左右的电压,但未接入TVP5151芯片时STM32单片机自身管脚时可以拉低的。TVP5151芯片供电正常,各管脚无短路。请问这是什么问题呢?
电路图是参考TVP5151手册绘制的。tvp5151原理图.pdf
您好,REST仅在PDN=1的时候使用,也就是TVP5151正常工作时(PDN低有效,当PDN=0时,TVP5151进入低功耗状态)才能使用reset复位功能。
我看电路中PDN和camera的PDN接在一起了,上电已经完全起来将PDN拉高了吗?
与电路中连接器连接的主要是STM32芯片HDMI接口和一些自定义引脚,上电后STM32将PND引脚拉高了的。
那上电期间,reset是否能由低到高变化?
还是只是在TVP5151正常操作期间,将其拉低不行,最低到2.2V是吗?
是的。rest是有高低变化的,但拉低时最低就到2.1~2.2V。
那就是高阻态呢。IO_DVDD 是3.3V,高电平最小值也是0.7*IO_DVDD=2.31V.
建议和camera的reset断开, 单独测试TVP5151的REST引脚,判断下时序是否正常?
单独给TVP5151供电时(不与STM32连接),REST管脚电压为2.4V。
单独给TVP5151供电时(不与STM32连接),REST管脚电压为2.4V。
您的意思是单独给TVP5151供电,reset悬空测得2.4V电压吗?
那如果没办法将rest拉低,是无法将TVP5151的上电时序完成的。
能否将TVP5151的上电时序,包含REST的时序波形附上我这边看下?
另外,有没有更换一片TVP5151试试?
是的,RESST悬空测得2.4V。
更换过TVP5151芯片,还是一样的情况。

蓝色是3.3V供电管脚上电时波形,黄色是REST管脚上电时波形。
不知是否和您的上电时序有关,看波形供电电压和REST同时拉高,这是不允许的,REST至少要在供电电压上电20ms之后再将REST拉高才能保证TVP5151的正常工作。参考下面的上电时序,也就是说t1(min)=20ms。

但这是我只给TVP5151供电时的时序,其它引脚均未与单片机连接进行操作。我还在5151的REST引脚上焊接了一个4.7kΩ的下拉电阻也无法将其拉低。
一上电就被拉高了,那肯定是不正常的,您在哪里购买的?
如果不是在TI购买的,建议可以申请样片再试试。