您好!想问下DP83620要配置为光口除了将硬件FX_EN_Z引脚通过2.2K电阻接地外,寄存器还需要进行配置吗?
我们现在电口能够正常通信,通过2.2K电阻将FX_EN_Z引脚接地,使用光口,可是光口不能通信,这是为什么?
还有就是发送端50Ω的上拉电阻是必须的吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好!想问下DP83620要配置为光口除了将硬件FX_EN_Z引脚通过2.2K电阻接地外,寄存器还需要进行配置吗?
我们现在电口能够正常通信,通过2.2K电阻将FX_EN_Z引脚接地,使用光口,可是光口不能通信,这是为什么?
还有就是发送端50Ω的上拉电阻是必须的吗?
具体的问题就是,当我由电口切换为光口是,单片机不能对620写数据,不能进行配置……!在线等回答,谢谢了!
今天晚上有测试了一下,发现RX端的电平一个为2.0,一个为2.4,TX端的电平一端为2.0,一端为1.997,按理来说我上拉接82Ω,下拉接130Ω电平应该是一样的,可为什么会有这么大的差距呢,还有一点就是,另外一块使用相同光模块的板子,测得RX端电平为1.996和1.996,TX则为1.640和1.640V,他们之间连接通讯不成功的原因会不会是因为他们之间的电平差引起的?求解答,谢谢了!