Other Parts Discussed in Thread: DP83620
各位大神,你们好!我使用的dp83620在硬件配置为光口的时候,出现单片机不能读写620的寄存器,但是当硬件配置为电口的时候,电口能够正常工作,想请教一下各位,这是这么回事?谢谢了…………!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: DP83620
各位大神,你们好!我使用的dp83620在硬件配置为光口的时候,出现单片机不能读写620的寄存器,但是当硬件配置为电口的时候,电口能够正常工作,想请教一下各位,这是这么回事?谢谢了…………!
你好!谢谢你的回答,我这个读写问题已经解决了,就是上电后,我需要对83620进行手动复位。
我们这边使用的MCU是stm32,我们是和以太网交换芯片的光模块通信的。
我想问下,那个光模块的上下拉电阻是像demo板上的一样上拉130,下拉82欧姆的吗?
还有只有TX需要104的电容耦合吗,RX使用为内部集成了104的交流耦合吗?
对于LVPECL电平,其基准电平为2V,也就是说3.3V供电的话需要3.3-1.3V啊,对于交流耦合是不是上拉82,下拉130,对于直流耦合是不是上拉130,下拉82,,
因为最终他们的直流偏置电压均在2.0V左右的对吗?
要是按照上面的分析,是不是那个demo板上的电路就是有问题的啊?
谢谢回答!
DP83620的Demo板电路应该有误,不管是直流耦合,还是交流耦合,LVPECL的共模电压为2V,你说的对,上拉电阻应该是82ohm,下拉是130ohm。