This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB8020B-Q1: usb20可以正常工作,但USB30无法正常工作,提示usb usb2-port1: Cannot enable. Maybe the USB cable is bad?

Part Number: TUSB8020B-Q1


usb20可以正常工作,但USB30无法正常工作,提示usb usb2-port1: Cannot enable. Maybe the USB cable is bad?

  • 您好,USB3.0无法工作指的是下行端口的接的是USB3.0的device无法工作是吗?

    那么和上行端口连接的是否能支持USB3.0? 因为如果和上行端口连接的USB端口只能支持2.0的话,那么下行端口是不支持USB3.0的,也最多只能支持到USB2.0.

    同样,如果和上行端口连接的只能支持低速或中速的话 ,那么下行端口USB3.0和高速也都是不支持的。

    除了上述情况,那也可能和cable有关,可以尝试更换一根cable试试。