This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI I2C/SMB Isolators ISO1541 技术问题

Other Parts Discussed in Thread: ISO1541

Hi TI 各位好

目前在使用 ISO1541(I2C/SMB Isolators)上遇到一些问题, 希望协助.

问题是I2C/SMB资料传输时, data(SDA1)之VOL1的电压偏高(约770~800mV).

在参考TI ISO1541的datasheet page4的规格为650~800mV后, 检验确认电路实测电压会常态的处于上限电压值.经调整R1阻值发现,

下图A点位置会随pull-high电阻变化而上下浮动.但无法降低SDA之VOL位准.

担心这个高的low level对于某些IC( 例如Microchip的PIC18 MCU )有误判的可能性.(datasheet page441)

ww1.microchip.com/.../41412F.pdf

是否有调整(降低)这个位准的方法.(避免让电位处于650~800mV上限)

谢谢

目前放10K VR, 10K~100都有去试看过电压波型变化.

VCC1与VCC2分别独立供电, 两侧均提供3.3V电压.